2024-10-18 1:58 PM
Hello! I believe I found a code generation bug. I am currently using IDE version 1.16.1.
By default, when enabling ADC with an STM32U5, HAL_MSPInit() has the line: HAL_PWREx_EnableVddA() which is necessary to have a positive reference for the ADCs (the U5 series has some internal switch to enable VDDA)
However, when enabling the feature "Generate peripheral initialization as a pair of '.c/.h' files per peripheral", the generated code removes the VDDA Enable line from HAL_MSPInit(). This makes the same ADC code fail to start (and lead to many hours of debugging).
Hoping someone at ST can confirm this (and push a fix) to confirm the root cause!
Solved! Go to Solution.
2024-10-19 12:17 AM - edited 2025-03-06 3:24 AM
Hello @rgangwan and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I confirm this code generation error, and I've escalated for correction on the future (under internal ticket number 186561).
PS: Issue solved on the last release of the STM32CubeMX
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-19 12:17 AM - edited 2025-03-06 3:24 AM
Hello @rgangwan and welcome to the ST Community :smiling_face_with_smiling_eyes:.
I confirm this code generation error, and I've escalated for correction on the future (under internal ticket number 186561).
PS: Issue solved on the last release of the STM32CubeMX
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-21 2:06 AM