2024-07-26 12:48 AM
Currently the behaviour of CubeIDE is to always choose the same build configuration for the Run and Debug button.
Is there a way to have the two seperated? Most of the time I want to flash the Debug build for debugging and the Release build with stronger optimizations when clicking Run.
It got me confused quite some times already, why the current consumption of the target is so incredible high after flashing code with "Run", until I remembered that I had a debugging session before and now the build config for the "Run" button was changed to Debug config...
So, is there a way to have the two buttons not change build config simultaneously but keep them separate?