2024-06-12 2:34 AM
Hello,
I will debug a application on the STM32G030F6 which are use to 90% the low poer sleep mode. For this I will show the changes of variables in RAM and Flash also the changes of SFR from the MCU hardware like SPI in real time. I will also manipulate variables in the RAM.
Now I see in the "Live Expression" view frosen values. The changes of the values are verry short.
How can I change the update period of the SFR and "Live Expression" view?
Thanks for our help,
Bernd
2024-07-05 3:05 AM
Hello @bm2 ,
If I understand your request well, you want to change the period of updating values in SFR view and live expression not at the same time.
This is not supported in STM32CubeIDE, but it could be a change request in the tool. So, could you specify the need more by attaching screenshots or zipped video?
Thanks,
Rim.
2024-07-09 9:48 PM
Hello Rim,
sorry no. I will not configured different period. I will configure a period. I don't see this in the configuration.
Thanks, Bernd