2024-05-03 02:16 AM
I am fresher here for the ST cube IDE i am trying to debug my code but it showing this error msg
Solved! Go to Solution.
2024-05-04 04:28 AM
So try with CubeProgrammer , connect, and show screenshot .
Info: with fake st-link V2 it won't work .
But we see then, what it's telling .
2024-05-03 03:08 AM
Is the gdb server set up? Did you try to start the gdb server manual? Does the Cube IDE command sequence point to the right places?
Probably there is also a log windows somewhere. Output there will help more than the pop-up.
2024-05-03 09:38 PM
Everything looks fine on the server side. it also follow command sequence to right places. can't find log windows
2024-05-04 12:38 AM
Dont see something in console output ?
->
+
What you set in debug settings for your project ?
2024-05-04 02:25 AM
This is my console output.
The debug settings are
2024-05-04 02:45 AM - edited 2024-05-04 02:46 AM
What is your st-link? The V2 stick?
Try connect: with type: software reset.
2024-05-04 03:27 AM
yes, The V2 stick
tried with software reset still facing the same
2024-05-04 04:28 AM
So try with CubeProgrammer , connect, and show screenshot .
Info: with fake st-link V2 it won't work .
But we see then, what it's telling .