2021-07-22 6:54 AM
Hello,
I'm working on a STM32H753 with STM32CubeIDE 1.4.0.
I have created an empty "STM32 Cortex-M C/C++ Application project". My executable is built by a separate makefile (arm-none-eabi-gcc based). I only use STM32CubeIDE to debug through a remote GDB server.
This setup has been working fine for a long time. Now I changed the memory mapping of my code. Before the code was executing from ITCM RAM and now I moved it to AXi-SRAM. Of course the code is copied from Flash to RAM by a kind of bootloader.
Now breakpoints seem to not work properly. They still work fine in the bootloader (in Flash) but as long as I set a bkpt in AXI SRAM the code doesn't stop. I checked that the assembly is correct. When I break in my code, I can see the correct assembly at the correct adress.
I tried to set bkpt through the GUI and through GDB commands it's the same.
Is there a particularity or a limitation regarding bkpt in AXI SRAM ?
thank you