2024-05-21 09:04 PM
Hello all,
We are trying to evaluate the STM32H735IG for our product. We bought the off-the-shelf dev kit and tried flashing it using S32CubeIDE, but encountered an error. The weird thing is, I can use S32 programmer to read flash, so the ST-Link seems to be up-to-date. I feel there is something wrong with S32CubeIDE. Can you please help.
All the versions are below and also some screenshots to assist help debugging
STM32CubeIDE
Version: 1.14.0
Build: 19471_20231121_1200 (UTC)
OS: Linux, v.6.5.0-27-generic, x86_64 / gtk 3.24.33
Java vendor: Eclipse Adoptium
Java runtime version: 17.0.8.1+1
Java version: 17.0.8.1
Logs in the error window
Error in final launch sequence:
Failed to execute MI command:
load /home/STM32CubeIDE/workspace_1.14.0/BSP/STM32CubeIDE/Debug/BSP.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load /home/STM32CubeIDE/workspace_1.14.0/BSP/STM32CubeIDE/Debug/BSP.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load /home/STM32CubeIDE/workspace_1.14.0/BSP/STM32CubeIDE/Debug/BSP.elf
Error message from debugger back end:
Load failed
Load failed
Logs in the console
STMicroelectronics ST-LINK GDB server. Version 7.5.0
Copyright (c) 2023, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Shutting down...
Exit.
2024-05-21 09:23 PM
Hello @Elimathew72 and welcome to the ST Community 😊.
Could you try this using the last version of STM32CubeIDE (V 1.15.1).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-05-22 10:33 AM
Still the same. I upgraded Stlink to the latest version too
STM32CubeIDE
Version: 1.15.1
Build: 21094_20240412_1041 (UTC)
OS: Linux, v.6.5.0-27-generic, x86_64 / gtk 3.24.33, WebKit 2.44.0
Java vendor: Eclipse Adoptium
Java runtime version: 17.0.8.1+1
Java version: 17.0.8.1
STMicroelectronics ST-LINK GDB server. Version 7.7.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Shutting down...
Exit.
2024-05-22 10:39 AM
Can still erase via stm32cubeprogrammer attaching a screenshot
2024-05-23 12:00 AM
Working here...
As long as my source code uses the SMPS:
HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY);
2024-05-23 09:04 AM
Hello We are trying the flash the sample off the example called BSP which blinks led.I don't see why this would affect connecting to stlink. Also many folks have experienced this problem but there is not concrete solutions.
2024-05-23 09:31 AM
Also tried @mattias norlander solution in https://community.st.com/t5/stm32cubeide-mcus/how-can-i-remove-error-like-waiting-for-debugger-connection/td-p/250559 to include debug configuration > Startup tab > Initialization commands > Add: monitor flash mass_erase in the startup script. The Mass erase is successful then it shuts down connection
STMicroelectronics ST-LINK GDB server. Version 7.7.0
Copyright (c) 2024, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.16.0
-------------------------------------------------------------------
Log output file: /tmp/STM32CubeProgrammer_5yyIDP.log
ST-LINK SN : 0037002A3137511433333639
ST-LINK FW : V3J15M6
Board : STM32H750B-DK
Voltage : 3.27V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 128 KBytes
Start Address : 8000000
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x90
Mass erase ...
Mass erase successfully achieved
Shutting down...
Exit.
2024-05-23 07:53 PM
The other datapoint is I have STM32F429I discovery kit and it flashes with no problem
2024-05-23 08:04 PM
The difference between STM32F429I discovery kit and STM32H750B-DK discovery kit is the stlink. Former has STLINK-V2 and the latter has STLINK-V3. Folks it'll be really helpful if anyone can assist me.
2024-05-23 08:40 PM