2023-12-21 01:42 AM
Hello all,
I can't download the STM32CubeIDE even as I am registered. There seems to be somthing broken with the Web page. I have tried several browsers. This is what I get, so there is no download button and the table is garbled:
Any help appreciated.
Johannes
Solved! Go to Solution.
2024-09-05 05:58 AM - edited 2024-09-05 06:03 AM
still not work till today (Sep 2024). It works only sporadically.
Work around is simply download as guest. The link will send to email.
2024-09-17 06:43 AM
I've never seen in my whole life a website that struggle to generate a download link so much
This is catastrophic for a company like this
2024-09-17 07:00 AM
Download as a guest is also not working..the provided link drives the st-site into an infinite loop which never times out. I've spent the whole day with different endless loops on the st-server.
It is absolut fruistrating!
One recommendation to ST:
Before thinking about adding AI features to the toolchain, do the more simple job and fix the server!
2024-09-25 08:40 AM
This is still broken..... After trying a couple different browsers the 4th or 5th attempt in firefox it suddenly worked. Very disappointing that something as simple as downloading a file is not working on STs website correctly. And it takes several minutes to load the download sections.