cancel
Showing results for 
Search instead for 
Did you mean: 

Can't download STM32CubeIDE

eble
Associate

Hello all,

I can't download the STM32CubeIDE even as I am registered. There seems to be somthing broken with the Web page. I have tried several browsers. This is what I get, so there is no download button and the table is garbled:

eble_0-1703151708265.png

Any help appreciated.

Johannes

 

19 REPLIES 19

still not work till today (Sep 2024). It works only sporadically.

Work around is simply download as guest. The link will send to email.

abonv
Associate

I've never seen in my whole life a website that struggle to generate a download link so much

This is catastrophic for a company like this

Download as a guest is also not working..the provided link drives the st-site into an infinite loop which never times out. I've spent the whole day with different endless loops on the st-server.

It is absolut fruistrating!

One recommendation to ST:

Before thinking about adding AI features to the toolchain, do the more simple job and fix the server!

aallardMVP
Associate

This is still broken.....  After trying a couple different browsers the 4th or 5th attempt in firefox it suddenly worked.  Very disappointing that something as simple as downloading a file is not working on STs website correctly.  And it takes several minutes to load the download sections.

flexiblebird
Associate

Yes, same situation on 10/11/24. ST does not seem interested in fixing it,

but vigorously prevents STM32CubeIDE-Win from being available at other download places.

I have a new computer, Win11 right out of the box, and are using Chrome 129.0.6668.100. 

 

But I have a solution: Try using Edge instead, and it finally works !

ST doesn't like Chrome.

 

slawekme
Associate

I was in need of quick download and setup STM32CubeIDE to provide support to one of my old customers. And guess what? Download doesn't work for me either. Spent several hours of my precious time trying different browsers, PCs, on Windows, Linux, even Android, as registered user and as a guest, directly and via VPN. Nope. Always the same result - after requesting download, the download does not start and the browser returns to the download page. No error message, nothing. This seems to be a problem of the server, not the client side.
ST, shame on you for this problem being persistent so long time. I'm now considering to tell my customers not to choose ST anymore.

You didn't understand. I was NOT able to download it despite I have tried hard. Nothing works.

good joke... at least with the linux stm32cubeide, guess what  they are shipping with it? a complete memory and cpu hooking chome...

Alon
Associate

Still a problem. what the hell

Alon
Associate

This link here sends to another portal from which the download works.

https://www.st.com/content/st_com/en/stm32cubeide.html#st-get-software

Praise be.