2024-06-21 01:43 AM
Every time I try to build a project, it says that build has finished but the process never actually finishes it stays at 98%, which prevents me from doing anything else.
I have to close cube and re-open it in order to build, it will finish once and then do this the second time.
2024-06-24 02:31 AM
Hello @Ryan-SmartIR
First let me thank you for posting.
Could you provide the .log found under /workspace/.metadata folder. This will help identify the root cause of this behavior.
Also, it would be helpful to know the IDE version you are working with and the debug configuration for your project.
Finally, does this behavior is systematic for any project you create and if you have tested with a new workspace.
BR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.