Skip to main content
JamB
Visitor II
May 13, 2020
Question

Build error VFP register argument (STM32F303RE nucleo board)

  • May 13, 2020
  • 0 replies
  • 797 views

Hi, I'm trying to use the console in CubeIDE with my STM32F303RE nucleo board and use printf(). For this, I chose an empty project, not STMCube. In the tool settings, I set floating-point unit to none and Floating-point ABI to Software implementation. Then in the syscall.c , I added to following code snippet below.

//Debug Exception and Monitor Control Register base address
#define DEMCR 			*((volatile uint32_t*) 0xE000EDFCU )
 
/* ITM register addresses */
#define ITM_STIMULUS_PORT0 	*((volatile uint32_t*) 0xE0000000 )
#define ITM_TRACE_EN 	*((volatile uint32_t*) 0xE0000E00 )
 
void ITM_SendChar(uint8_t ch)
{
 
	//Enable TRCENA
	DEMCR |= ( 1 << 24);
 
	//enable stimulus port 0
	ITM_TRACE_EN |= ( 1 << 0);
 
	// read FIFO status in bit [0]:
	while(!(ITM_STIMULUS_PORT0 & 1));
 
	//Write to ITM stimulus port0
	ITM_STIMULUS_PORT0 = ch;
}
 
__attribute__((weak)) int _write(int file, char *ptr, int len)
{
	int DataIdx;
 
	for (DataIdx = 0; DataIdx < len; DataIdx++)
	{
		//__io_putchar(*ptr++);
		ITM_SendChar(*ptr++);
	}
	return len;
}

Before adding this code to syscall.c, I could build the project without any error. However, after adding the definitions and ITM_SendChar function I cannot build the project.

I get the following error.

c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe: error: Src/sysmem.o uses VFP register arguments, 001HelloWorld.elf does not
 
c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe: failed to merge target specific data of file Src/sysmem.o
 
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:43: 001HelloWorld.elf] Error 1
"make -j4 all" terminated with exit code 2. Build might be incomplete.
 
14:16:25 Build Failed. 1 errors, 0 warnings. (took 1s.325ms)

Any ideas, how can I get rid of VFP register arguments and use the printf()?

Thanks for your help in advance.

This topic has been closed for replies.