2024-03-19 07:42 PM
Hi.
I was using STM32CubeIDE 1.14.0 until yesterday.
Build Analyzer worked fine in 1.14.0, but after updating to 1.15.0 using the update feature provided by CubeIDE, nothing is displayed in Build Analyzer.
The build was successful and the <project>.map file was created, but the Build Analyzer information was not displayed, and I uninstalled and reinstalled CubeIDE, but it was the same.
Solved! Go to Solution.
2025-02-10 03:36 AM
If you've opened a second Eclipse window it also will not work. You'll have to restart Eclipse in that case.
2025-02-10 05:38 AM
Is the code for this plugin available?