cancel
Showing results for 
Search instead for 
Did you mean: 

Azure RTOS for STM32U599

MichaelW
Associate II

Hello again,

After configuring all of the peripherals and pins, I have run into another problem.  I need to enable the Azure RTOS but I don't have any selection for U5.  I am on the latest build now and I downloaded the latest FW package (1.3.0). I'm using the STM32U599VJT6.

I see others talking about using it and there are videos about it so I must be doing it wrong.  Is there a package that I am not seeing is missing?  I am using Azure for an H7 project but it was a while ago so maybe I'm just missing something with this new chip!

 

Thanks so much!

 

Michael

1 ACCEPTED SOLUTION

Accepted Solutions
Issamos
Lead II

Hello @MichaelW 

As you can see in the following wiki. All new series released in 2021 and later (including the U5 serie) are covered by default by Azure® RTOS MW within the matching STM32Cube MCU packages. So no need to add  any other middleware (as you used to do withe the H7 serie).

Best regards.

II

View solution in original post

3 REPLIES 3
Issamos
Lead II

Hello @MichaelW 

As you can see in the following wiki. All new series released in 2021 and later (including the U5 serie) are covered by default by Azure® RTOS MW within the matching STM32Cube MCU packages. So no need to add  any other middleware (as you used to do withe the H7 serie).

Best regards.

II

MichaelW
Associate II

Thank you again for the continued fast support!  I guess it really was different with the H7.  I won't pretend to be an expert with each change and so perhaps this is just adding the ThreadX option from the "middleware and software packs" selections.  I'm going to keep digging into this and would like to leave this discussion open, in case I have more questions on this, if that is okay.

 

Thanks again!

 

Michael

Hello again @MichaelW 

I will be always happy to help if i can. But i Suggest you to close this topic by choosing a best answer and than ask your next questions in a new post to give them more visibility and more people can give help.

Best regards.

II