2022-10-26 2:17 AM
Hello,
I've designed a board with the MCU above. The board has the following peripherals/configurations:
-i2c
-spi
-gpioA
-gpioB
-EXTI and timer interrupts
-serial wire debug
-timers (tim2, tim21, tim22)
The board has some ICs that are all in their lowest power state. I estimate a total of 100uA spent on these ICs.
The code itself initializes the peripherals and sets SPI and I2C devices into their lowest power states before entering the main loop, which is empty.
I acknowledge that the other IC's on the board and the peripherals that are not associated with a clock will drain a roughly constant current. My confusion is regarding how the consumption of the board scales with the MSI clock. Below is my data.
Clock speed (kHz) | Board current (uA)
4194 | 2330
1048 | 1275
524 | 850
As you can see, the current consumption appears to be something like:
current = M*clock + static drainage, where M is much larger (~4X) than the datasheet suggests.
Any suggestions would be greatly appreciated.
Best,
Oliver
2022-10-26 2:35 AM
Try first with an empty loop, no peripherals initialized.
JW
2022-10-26 12:16 PM
Hi JW,
I've removed all code such that SystemClock_Config(); and HAL_Init(); are the lines run before an empty loop. Here is my results:
4mhz = 1603
1mhz = 1217
0.5mhz = 1150
If I add the gpio initialize and set the board ICs into their lowest power mode (via gpio outputs) I obtain:
4mhz: 1365
1mhz: 929
0.5mhz: 856
These sorts of changes are consistent with the datasheet, with the gpio version understandably having slightly higher changes. We can also see from the tests that the non-mcu IC's use roughly 250uA more when not powered down.
I have two questions from here:
1) Why are the peripherals using so much current? The STM32CubeIDE tool shows that the peripherals should draw, for example, 130uA at 4mhz, not 727 uA.
2) The board itself should not be using 800uA in its powered down state. Are there sources of constant current draw within the mcu that I can optimize?
Thank you.
Best,
Oliver
2022-10-27 9:08 AM
Hi Oliver,
I don't want to delve into the particularities of your design, that's your job.
Try a Nucleo board as a "known good" reference point.
Set the mcu to some of the lowest-consumption "sleep" modes to compare consumption with rest of the board. Don't forget that debugging may be intrusive also in low power modes and may influence consumption (not only in those modes).
Try to disconnect/remove parts (or add them incrementally) to find out what causes the excessive current.
Try adding/removing handling of peripherals for the same purpose.
JW