2024-05-19 7:53 AM
I don't know if this is caused by the vscode extension or stm32cubeclt, but after the installation(everything related to the extension works), I noticed that the system path variable had been modified to add stm32cubeclt bin directories(I found this script: /etc/profile.d/cubeclt-bin-path_1.15.1.sh).
Is this normal? I want to use my system default cmake, is there a workaround instead of using /usr/bin/cmake every time?
I'm using debian 12.
Solved! Go to Solution.
2025-10-21 2:36 AM - edited 2025-10-21 2:40 AM
Hi @Tizio1234 and @ecorm ,
No doubt developers are doing more than only STM32 development. Many companies are multi-sourcing MCUs within the same project for multiple reasons. Or developing C/C++ applications to be running on the host PC.
Regardless our STM32 tool ecosystem cannot collide with whatever you want to do. When distributing our new CLI tools one challenge is to ensure that some contradicting requirements are fulfilled:
The new approach: Instead of polluting your environmental variables on your system, the new solution instead brings a "cube-wrapper" offering a managed cube CLI toolbox. You can run commands from inside an STM32 project context and ensure the right CLI tools of the right versions are called... As example:
We are not 100% there yet, but this is the direction we are selecting to encompass your need to have a good out-of-the-box experience, guarantee re-producibility, while not tainting your system, nor colliding with other tools you have on your PC.