cancel
Showing results for 
Search instead for 
Did you mean: 

STLink GDB Server 1.3.0 breaks support on STM32G473CET3

devrim6
Associate

As the title says, the most recent 1.3.0 version of the extension breaks functionality of the debugger for the STM32G473CET3 MCU (and possibly others). By "breaks functionality", I mean that it does not even connect to the MCU anymore.

4 REPLIES 4

Unfortunately it does not :(

The specific error I get is the usual

the system tried to join a drive to a directory on a joined drive

that happens on a variety of problems.

Hi @devrim6,

Is there a more explicit message in the debug console view?

It is possible to add a `"verbose"` attribute set to `true` in the debug configuration to add even more logs to the debug console.

Regards,

Elliot

@devrim6 

Have you updated project locked bundles ? Updating system local bundles repository is not enough ...