Skip to main content
Associate
May 5, 2026
Solved

Debug STLink GDB Server v.1.3.0 - PARSE ERROR: Argument: -cp

  • May 5, 2026
  • 5 replies
  • 420 views

Hello,

I'm sorry to bother again, but it seems there is another issue in the latest update of VSCode STM32IDE extension. While trying to Start Debugging with GDB Server (STM32Cube Debug STLink GDB Server v1.3.0), with launch.json as:

 "version": "0.2.0",
 "configurations": [

 {
 "type": "stlinkgdbtarget",
 "request": "launch",
 "name": "STM32Cube: STM32 Launch ST-Link GDB Server",
 "origin": "snippet",
 "cwd": "${workspaceFolder}",
 "serverReset": "Connect under reset",
 "preBuild": "${command:st-stm32-ide-debug-launch.build}",
 "runEntry": "main",
 "imagesAndSymbols": [
 {
 "imageFileName": "${command:st-stm32-ide-debug-launch.get-projects-binary-from-context1}"
 }
 ],
 "faultUnalignedAccess": false,
 "liveWatch": {
 "enabled": true,
 "samplesPerSecond": "4"
 },
 "preRunCommands": [
 "set output 16"
 ]
 }
 ]
}

 The Debug starts and I get an error message as:

PARSE ERROR: Argument: -cp (--stm32cubeprogrammer-path)
 Argument already set!

Brief USAGE: 
 C:/Users/.../AppData/Local/stm32cube/bundles/stlink-gdbserver/7.10
 .0+st.3/bin/ST-LINK_gdbserver.exe 
 [--external-init]
 [--pend-halt-timeout <Pending halt
 timeout>] [--halt] [-c <config
 file>] [-e] [-f <log file>] [-l
 <log level>] [-p <port number>]
 [-v] [-r <refresh delay>] [-s] [-d]
 [-z <port number>] [-a <cpu clock>]
 [-b <SWO CLOCKDIV>] [-k] [-q] [-i
 <ST-LINK S/N>] [-m <apID>] [-g]
 [-t] [--erase-all] [--memory-map
 <device id>] [--ext-memory-loaders]
 [-ei <file_path>] ... [-el
 <file_path>] ... [-cp <path>]
 [--temp-path <path>]
 [--preserve-temps] [--frequency
 <max freq kHz>] [--licenses] [--]
 [--version] [-h]

For complete USAGE and HELP type: 
 C:/Users/.../AppData/Local/stm32cube/bundles/stlink-gdbserver/7.10.0+st.3/bin/ST-LINK_gdbserver.exe --help

cube has exited with code 1GNU gdb (GNU Tools for STM32 13.3.rel1.20250523-0900) 14.2.90.20240526-git
Copyright (C) 2023 Free Software Foundation, Inc.
License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>
This is free software: you are free to change and redistribute it.
There is NO WARRANTY, to the extent permitted by law.
Type "show copying" and "show warranty" for details.
This GDB was configured as "--host=x86_64-w64-mingw32 --target=arm-none-eabi".
Type "show configuration" for configuration details.
For bug reporting instructions, please see:
<https://www.gnu.org/software/gdb/bugs/>.
Find the GDB manual and other documentation resources online at:
 <http://www.gnu.org/software/gdb/documentation/>.

 If I switch to older version v1.2.0, there is no issue.

I'm using STLink V3SET. I have tried to generate new STLink GDB Server Configuration, but the issue is still there on v1.3.0. Also I have tried to: Set Up STM32Cube project(s) again, with no luck too.

Thanks for looking into it.

Best answer by Florent V

Hi @Michael12 , @dalbiero-BW 
I see @Michael12 that you are using ST-Link GdbServer 7.10.0+st.3 with your project.
Is it the same for you @dalbiero-BW ?

Could you please open the bundle manager of your project ("STM32Cube" activity bar > "stm32cube bundle manager" view in the left panel) and update the ST-Link GdbServer for your project?
Please also update to the latest available programmer.

Kind regards,
/Flo

5 replies

Visitor II
May 5, 2026

I have the same problem.

Florent V
Florent VBest answer
ST Employee
May 5, 2026

Hi @Michael12 , @dalbiero-BW 
I see @Michael12 that you are using ST-Link GdbServer 7.10.0+st.3 with your project.
Is it the same for you @dalbiero-BW ?

Could you please open the bundle manager of your project ("STM32Cube" activity bar > "stm32cube bundle manager" view in the left panel) and update the ST-Link GdbServer for your project?
Please also update to the latest available programmer.

Kind regards,
/Flo

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Michael12Author
Associate
May 6, 2026

Thank you, works fine now!

Visitor II
May 5, 2026

I updated `stlink-gdbserver` to 7.13 and `programmer` to 2.22 and now everything works!

Florent V
ST Employee
June 17, 2026

Hi,

 

For users experiencing this issue who have not updated the bundles ST-Link GdbServer and Programmer, the new release of our VSCode extensions resolves the problem. Therefore, updating the bundles is no longer necessary for this use case unless you choose to do so.

 

Kind Regards,
/Flo

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.