2025-11-05 10:43 AM - last edited on 2025-11-05 11:31 AM by Andrew Neil
Hi,
I followed the directions to create an empty project in VSCode. I picked my device, an F405RGT6, and the extension did what it did. Now what? The docs end there. If I launch MX from inside VSCode, MX wants an ioc file; there isn't one to find. What shall I do? Thanks.
2025-11-05 10:57 AM
2025-11-05 11:34 AM
If you want to work with CubeMX, then start in CubeMX and use it to create the project.
Creating a blank project assumes that you're going to fill in everything yourself, from scratch.