2024-02-29 3:19 PM
I was using the SystemWorkbench for years and everything OK. Recently changed to STM32CubeIDE and also able to build and debug within hours with released ST project "STM32Cube_FW_F4_V1.28.0".
Have tried to use the new "STM32 VS Code Extension" in VSCode as it is getting popular.
1. Followed the instructions to install "STM32CubeCLT", note : I installed in different location "C:\Tools\STM\STM32CubeCLT"
2. Modified the "WINDOWS_ST_CLT_PATH" and "TOOLCHAIN_DIRECTORIES" in gcc-arm-none-eabi.cmake, and the project is built successful - OK.
3. Try to "Debug" the project but it shows error message :
Questions :
For STM32CubeIDE, it is using OpenOCD.
For VSCode, How to configured and setup to use the Debug Tools under STM32CubeCLT ?
Thanks
Solved! Go to Solution.
2024-03-01 8:33 AM
Issue resolved by re-installed both
- STM32CubeIDE and STM32CubeCLR to default location "C:\ST"
Looks like both tools are inter-connected to each other in un-documented manner.
2024-02-29 4:33 PM
Anyone knows how to update this for the Tools required for debugger ??
2024-03-01 8:33 AM
Issue resolved by re-installed both
- STM32CubeIDE and STM32CubeCLR to default location "C:\ST"
Looks like both tools are inter-connected to each other in un-documented manner.