Question
Can't include libraries in visual code studio
Hello,
I try to do a little code for STM32F103 MCU using Visual Code Studio with STM32 VS code Extension.
I can generate and compile base code using STM32CubeMX importation feature.
But I'm stuck with adding external libraries to the project.
What i've done is to modify the "c_cpp_properties.json" file of the project to add the path to the library I want to use.
Here the current file :
{
"version": 4,
"configurations": [
{
/**
* ms-vscode.cmake-tools plugin should be installed.
*
* It provides data for C/C++ plugin,
* such as include paths, browse paths, defines, etc.
*/
"name": "STM32",
"includePath": [
"lib/ssd1351"
],
"configurationProvider": "ms-vscode.cmake-tools",
//"intelliSenseMode": "${default}",
"intelliSenseMode": "gcc-arm"
}
]
}
But when I include the ssd1351.h header in the main.c file, it fail :
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "ssd1351.h"
/* USER CODE END Includes */
Can someone point me to the solution for including external libraries in an VScode project ?
Thank you