cancel
Showing results for 
Search instead for 
Did you mean: 

Is a more intensive support of the Zephyr ecosystem planned?

Amelie ACKERMANN
Community manager
Community manager

Currently, we are developing in two worlds using the STM32Cube *AND* the Zephyr RTOS ecosystem. It would help us a lot if Zephyr could be supported more intensively, e.g. generating a Zephyr device tree from an STM32Cube(MX) setup. Is a more intensive support of the Zephyr ecosystem planned?

2 REPLIES 2
Roman LUDIN
ST Employee

Hello, Currently the support in MX is not planed. But this of course depends also on the feedback like this. So I'll forward this feedback to our marketing department.

Tom_pm
Associate II

That would indeed be a very helpful feature, especially for people not yet familiar with device tree.


As far as I know it's already possible to generate Device tree files for STM32MP1 for quite a while, so maybe you could even built upon that.
Also, a different vendor(Name starting with N) has in the meantime quite a usable dts generation tool in their VS-Code extension, so you may take some inspiration from there as well