cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157CAA3T is not able to program and Boot

Heena
Associate

Hi,

We are using STM32MP157CAA3T processor. We have implemented USB, UART and SD card for Booting purpose.

And currently we are programming the processor via UART8 by using USB to UART convertor.

Used UART4 Debug port for troubleshooting the board.

Problem is that, we are not able to program the board. And also USB, UART and SD card are failing to boot the processor.

2 REPLIES 2
PatrickF
ST Employee

Hi @Heena 

need to give more details to allow a valuable answer.

I assume it is a custom board.

Did you successfully rebuilt the ecosystem based on your custom HW ?

Is it using STPMIC1 ?

Is it using HSE crystal or oscillator ?

Which DDR ? is DDR tested using DDRFW-UTIL ?

Could you share some console messages ?

 

Regards

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Christian N
ST Employee

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.