STM32 MPUs Solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP157CAA3T is not able to program and Boot

Hi,We are using STM32MP157CAA3T processor. We have implemented USB, UART and SD card for Booting purpose.And currently we are programming the processor via UART8 by using USB to UART convertor.Used UART4 Debug port for troubleshooting the board.Probl...

Heena by Associate
  • 144 Views
  • 3 replies
  • 0 kudos

Resolved! EMMC flash

is it possible to OpenSTlinux distribution Package SD card images , flashing directly on board(STM32MP157F -DK2) in EMMC. I do not want to use SD card for booting. please help me out this.

meta qt

how to add meta qt layers into our OpenSTlinux distribution package. please do step by step 

Resolved! wifi enabling problem

hi i successfully connecting wifi on STM32mp157f-DK2 board through IPhone but the when i pass the command "# ping google.com " then it show temporary failure  in name resolution ,  and also dhcp command not found why this is happen. please reach me o...

How to make STM32MP151 successfully run LINUXPTP

STM32MP151 is a PTP slave clock, and the master clock is correctly determined and configured. In the same network, multicast, E2E, and one-step configuration modes are used. Run ptp4l,Output prompt: "Received SYNC without timestamp". the actual SYNC ...

fudaguo by Associate II
  • 2090 Views
  • 4 replies
  • 0 kudos

Ethernet Ping issue in UbootV2022.10

Hello,We are using STM32157AAA3 Processor in our custom board and Microchip Ksz9893 switch for ethernet and the switch is configured using i2c.when we are trying to ping ethernet in RGMII mode in U-Boot v2022.10-stm32mp-r1 we are getting the Rx-clock...

eth_log.PNG Fixedllink_eth_log.PNG