cancel
Showing results for 
Search instead for 
Did you mean: 

EV1 & MB1379 Performance

Eldam
Senior

Hello ST Teams!

I'd like to know if someone have ever tried to get 1920*1080*30fps with the configuration above (STM32MP157C-EV1 and MB1379 board).

We'd like to achieve this performance, OV5640 datasheet camera says "ok for me"

v4l2 listing capabilities says "ok for me" :

               Size: Discrete 1920x1080

                       Interval: Discrete 0.067s (15.000 fps)

                       Interval: Discrete 0.033s (30.000 fps)

But if we try with dev board (OSD32BRK) and flying wires with camera(OV5640), fps is limited to 13fps.

My question is: Is it possible to achieve 30fps in this configuration?

we will reproduce schematics of (STM32MP157C-EV1 and MB1379 board) camera part

(dcmi + ext clk ) , but we're not sure of fps performance .

from: "dm00693021-stm32mp1-series-interfacing-with-a-mipi-csi2-camera-stmicroelectronics.pdf" (okay its using he STMIPID02 but commands are the same)

root@stm32mp1-av96:~# v4l2-ctl --set-parm=30;

root@stm32mp1-av96:~# v4l2-ctl --set-fmt-video=width=1920,height=1080,pixelformat=RGBP --stream-mmap --stream-count=-1

Can someone try it ?

1 ACCEPTED SOLUTION

Accepted Solutions
OlivierK
ST Employee

Hello Eldam (Community Member),

The Maximum DCMI performance that can be acheived with the STM32MP157 is 24Mpix/s with 16 bits per pixel using 8 bits parallel bus.

Therefore 13 fps that you've found for 1920x1080 resolution is correct.

Regards,

Olivier

View solution in original post

2 REPLIES 2
OlivierK
ST Employee

Hello Eldam (Community Member),

The Maximum DCMI performance that can be acheived with the STM32MP157 is 24Mpix/s with 16 bits per pixel using 8 bits parallel bus.

Therefore 13 fps that you've found for 1920x1080 resolution is correct.

Regards,

Olivier

Eldam
Senior

Hello Olivier,

Thanks for answering me.

By the time, we have been able to get 30fps by lowering resolution.

Have nice summer holidays!