2021-01-04 6:53 AM
I'm updating a .tsv file, used by the CubeProgramer to program a STM32MP DK1. The file I'm looking at contains:
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157a-dk1-serialboot.stm32
- 0x03 ssbl-boot Binary none 0x0 bootloader/u-boot-stm32mp157a-dk1-trusted.stm32
P 0x04 fsbl1 Binary mmc0 0x00004400 arm-trusted-firmware/tf-a-stm32mp157a-dk1-trusted.stm32
P 0x05 fsbl2 Binary mmc0 0x00044400 arm-trusted-firmware/tf-a-stm32mp157a-dk1-trusted.stm32
PD 0x06 ssbl Binary mmc0 0x00084400 bootloader/u-boot-stm32mp157a-dk1-trusted.stm32
P 0x21 boot System mmc0 0x00284400 st-image-bootfs-openstlinux-weston-stm32mp1.ext4
P 0x22 vendorfs FileSystem mmc0 0x04284400 st-image-vendorfs-openstlinux-weston-stm32mp1.ext4
P 0x23 rootfs FileSystem mmc0 0x05284400 st-image-weston-openstlinux-weston-stm32mp1.ext4
P 0x24 userfs FileSystem mmc0 0x33C84400 st-image-userfs-openstlinux-weston-stm32mp1.ext4
I'm trying to understand the file's contents and how to modify it correctly.
1) Is there any documentation on this file?
2) From playing with the file it seems, the "fsbl1-boot" and "ssbl-boot", appear to be an initial load used to flash the rest of the board. Is that correct?
3) When preparing images, how are the fsbl1-boot/ssbl-boot generated? When I ran a bootloader build, the output seemed to have been:
u-boot u-boot.cfg.configs u-boot.lds u-boot.srec u-boot.sym
u-boot.bin u-boot.dtb u-boot.map u-boot.stm32
u-boot.cfg u-boot-dtb.bin u-boot-nodtb.bin u-boot.stm32.log
Thanks.
Solved! Go to Solution.
2021-01-04 7:08 AM
Hi @MWors.1 ,
1) Did you visit our wiki ? eg https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout ?
2) Yes, right
3) This is output of uboot build. u-boot.stm32 can be used as ssbl-boot and ssbl.
For fsbl1 it's generated by TF-A with specific flavor "serialboot" for fsbl1-boot.
This is automatically generated when compiling tf-a with SDK
Hope it help,
Olivier
2021-01-04 7:08 AM
Hi @MWors.1 ,
1) Did you visit our wiki ? eg https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout ?
2) Yes, right
3) This is output of uboot build. u-boot.stm32 can be used as ssbl-boot and ssbl.
For fsbl1 it's generated by TF-A with specific flavor "serialboot" for fsbl1-boot.
This is automatically generated when compiling tf-a with SDK
Hope it help,
Olivier
2021-01-04 11:16 PM
Thanks for the input @Community member
For #1 that was the documentation I was looking for. Thank you.
For #3, Is there more information of compiling tf-a? I'm currently only using the standalone toolchain against the u-boot/kernel code base to generate images. Is the fsbl1 *only* generated via this "TF-A" process?
Thanks.
-Mike
2021-01-05 12:55 AM
Hi @MWors.1 ,
For #3 I guess you will found all you need there :
https://wiki.st.com/stm32mpu/wiki/STM32MP1_Developer_Package#Installing_the_TF-A
Olivier