2021-12-16 4:15 PM - last edited on 2023-07-11 9:37 AM by Kevin HUBER
I believe HSE is 24 MHz, DIVM3 is /2 (12 MHz) DIVN3 is X34 (408 MHz) DIVP3 is /2 (204 MHz) But the screen says it is 208.87793.
I thought I knew how the PLL worked. And it is not like this.
I have a screen shot.
Solved! Go to Solution.
2021-12-16 4:28 PM
You have a fractional N set in your PLL. Set it back to 0 to get the expected results.
2021-12-16 4:28 PM
You have a fractional N set in your PLL. Set it back to 0 to get the expected results.
2021-12-16 11:39 PM
@TDK gives the right answer. 24/2=12MHz, 12MHz*(34+6660/8192) = 417.755859MHz with DIVP3=2 end up to 208.8779297MHz.
Regards.
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'
2021-12-18 12:08 PM
I missed that completely. Thank you.
I do not remember changing it. And do not know why I would.
Thanks again.
Kip