cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX crashes when generating code for STM32MP151

dirk.schoebel
Associate

I have a complex project which i try to use CubeMX to generate the device trees for A-TF, OP-TEE and Linux, as well as code pieces for the M4.

The crash is not visible in the STM32CubeMX.log file, but is printed in stderr:

2022-04-14 14:55:51,876 [INFO] BlockDiagram:2740 - set Specific Code input for plugin: TAMP
2022-04-14 14:55:51,876 [INFO] BlockDiagram:2740 - set Specific Code input for plugin: ETH
2022-04-14 14:55:51,877 [INFO] CodeGenerator:663 - code generatio: config db path: /home/dirks/STMicroelectronics/STM32CubeMX_Pre//db/
java.lang.NumberFormatException: For input string: "LSI_VALUE"
        at java.base/jdk.internal.math.FloatingDecimal.readJavaFormatString(FloatingDecimal.java:2054)
        at java.base/jdk.internal.math.FloatingDecimal.parseFloat(FloatingDecimal.java:122)
        at java.base/java.lang.Float.parseFloat(Float.java:455)
        at com.st.microxplorer.codegenerator.McuDataModel.getIpRCCSourceInfo(McuDataModel.java:939)
        at com.st.microxplorer.codegenerator.McuDataModel.initMcuData(McuDataModel.java:221)
        at com.st.microxplorer.codegenerator.McuDataModel.<init>(McuDataModel.java:162)
        at com.st.microxplorer.codegenerator.CodeGenerator.generateCode(CodeGenerator.java:1220)
        at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.generateCode(ProjectBuilder.java:2369)
        at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createCode(ProjectBuilder.java:1961)
        at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:630)
        at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:54)

Doing the whole pin configuration for more than 100 pins is very time consuming. We are in the process of having a second project with the STM32MP1 (XXXXXXX removed by moderator), so the graphical tool would be extremely helpful.

I tried to generate the code with CubeMX 6.5.0, and also with the XXXXX (removed by moderator), both crash with the same error.

Regards,

Dirk.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
dirk.schoebel
Associate

The problem appears with the STM32MP151 project, independent of the second one.

johnnyc
Associate III

We're having exactly the same problem with a STM32MP157 project, stack trace is the following:

java.lang.NumberFormatException: For input string: "LSI_VALUE"
at java.base/jdk.internal.math.FloatingDecimal.readJavaFormatString(FloatingDecimal.java:2054)
at java.base/jdk.internal.math.FloatingDecimal.parseFloat(FloatingDecimal.java:122)
at java.base/java.lang.Float.parseFloat(Float.java:455)
at com.st.microxplorer.codegenerator.McuDataModel.getIpRCCSourceInfo(McuDataModel.java:939)
at com.st.microxplorer.codegenerator.McuDataModel.initMcuData(McuDataModel.java:221)
at com.st.microxplorer.codegenerator.McuDataModel.<init>(McuDataModel.java:162)
at com.st.microxplorer.codegenerator.CodeGenerator.generateCode(CodeGenerator.java:1254)
at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.generateCode(ProjectBuilder.java:2665)
at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createCode(ProjectBuilder.java:2094)
at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:752)
at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:54)

Can anyone from ST help out?

johnnyc
Associate III

@Community member​ Can you please have a look, this is urgent for one of our customers.

Sara BEN HADJ YAHYA
ST Employee

Hello @dirk.schoebel​ , @johnnyc​ 

Could you please share a detailed scenario to help me reproduce the issue ?

Thanks,

Sara.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.