cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX project generation fails for MP157D

0xdeadbeef
Associate II

Hello,

I am trying to generate a STM32CubeIDE project using CubeMX (version 6.16.1) for MP157D-DK1 board. It generates some device trees (linux, u-boot, tp-a) but it fails to generate the CubeIDE project.

I also tried older versions of CubeMX (as late as 6.12) and none work.

The error it displays is attached. Any idea what might be going wrong with the code/project generation? I have STM32CubeIDE v2.0.0 installed.

Thanks.

1 ACCEPTED SOLUTION

Accepted Solutions
Issamos
Lead III

Hello @0xdeadbeef 

You may find this post helpful.

Best Regards.

II

View solution in original post

3 REPLIES 3
Issamos
Lead III

Hello @0xdeadbeef 

You may find this post helpful.

Best Regards.

II

0xdeadbeef
Associate II

Allright, it seems that setting the hostname to "localhost" fixes the problem. I am also using openSUSE (Tumbleweed). Thanks.

0xdeadbeef
Associate II

Since this seems like a bug that is now over 3 years old and the workaround is working on openSUSE,I'll perhaps also try using Ubuntu/Fedora distrobox container for my STM tools to avoid further problems for the time being.