2020-06-22 2:03 AM - last edited on 2023-07-12 10:13 AM by Kevin HUBER
There are only a linux path suggested, no windows path. If windows is not supported, then it is not stated in previous steps. If it is supported, then path is missing at step 2.1
/Peter
2020-06-22 4:48 AM
Hi @PLied,
The MP1 Cube itself can also be used on Windows - for development of M4 core code.
But because most of development is running on Linux only the recommended path is for Linux.
See: https://wiki.st.com/stm32mpu/wiki/PC_prerequisites
So in windows you can place this package anywhere according your needs.
Best regards,
Milan
2020-07-01 7:05 AM
Well, I have been using IAR for decades and Cortex-M for quite some time so I will stick to what I am used to, Windows host for development. I prefer to use linux as virtual machines without desktop and use filesharing with windows where needed. Don't assume that there are only Linux desktops used by developers...