2025-07-19 1:22 AM - edited 2025-07-19 1:40 AM
Hello,
I have a problem with the U-Boot stuck and loading the Kernel
Here is my log
NOTICE: CPU: STM32MP151CAA Rev.Z
NOTICE: Model: STMicroelectronics custom STM32CubeMX board - openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11
INFO: PMIC version = 0x21
NOTICE: Reset reason (0x114):
INFO: IWDG1 Reset (rst_iwdg1)
INFO: FCONF: Reading TB_FW firmware configuration file from: 0x2ffe2000
INFO: FCONF: Reading firmware configuration information for: stm32mp_fuse
INFO: FCONF: Reading firmware configuration information for: stm32mp_io
INFO: Using SDMMC
INFO: Instance 1
INFO: Boot used partition fsbl1
NOTICE: BL2: v2.10-stm32mp1-r1.0(debug):lts-v2.10.5-dirty(7c229848)
NOTICE: BL2: Built : 16:19:31, Jun 28 2024
INFO: BL2: Doing platform setup
INFO: RAM: DDR3-DDR3L 16bits 466000kHz
INFO: Memory size = 0x20000000 (512 MB)
INFO: BL2: Loading image id 1
INFO: Loading image id=1 at address 0x2ffff000
INFO: Image id=1 loaded: 0x2ffff000 - 0x2ffff1ea
INFO: FCONF: Reading FW_CONFIG firmware configuration file from: 0x2ffff000
INFO: FCONF: Reading firmware configuration information for: dyn_cfg
INFO: FCONF: Reading firmware configuration information for: stm32mp1_firewall
INFO: BL2: Loading image id 4
INFO: Loading image id=4 at address 0x2ffc0000
INFO: Image id=4 loaded: 0x2ffc0000 - 0x2ffc002c
INFO: OPTEE ep=0x2ffc0000
INFO: OPTEE header info:
INFO: magic=0x4554504f
INFO: version=0x2
INFO: arch=0x0
INFO: flags=0x0
INFO: nb_images=0x2
INFO: BL2: Loading image id 8
INFO: Loading image id=8 at address 0x2ffc0000
INFO: Image id=8 loaded: 0x2ffc0000 - 0x2ffdebb8
INFO: BL2: Loading image id 9
INFO: Loading image id=9 at address 0xde000000
INFO: Image id=9 loaded: 0xde000000 - 0xde077000
INFO: BL2: Loading image id 2
INFO: Loading image id=2 at address 0xc0500000
INFO: Image id=2 loaded: 0xc0500000 - 0xc0513d20
INFO: BL2: Skip loading image id 16
INFO: BL2: Loading image id 5
INFO: Loading image id=5 at address 0xc0100000
INFO: Image id=5 loaded: 0xc0100000 - 0xc021e500
NOTICE: BL2: Booting BL32
INFO: Entry point address = 0x2ffc0000
INFO: SPSR = 0x1d3
I/TC: Early console on UART#4
I/TC:
I/TC: Pager is enabled. Hashes: 3936 bytes
I/TC: Pager pool size: 52kB
I/TC: Embedded DTB found
I/TC: OP-TEE version: 4.0.0-dev (gcc version 13.3.0 (GCC)) #1 Fri Oct 20 18:29:31 UTC 2023 arm
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: WARNING: All debug accesses are allowed
I/TC: Platform stm32mp1: flavor PLATFORM_FLAVOR - DT stm32mp151c-chargehub-mx.dts
I/TC: OP-TEE ST profile: secure_and_system_services
E/TC:0 0 call_initcalls:43 Initcall __text_start + 0x0003507c failed
I/TC: Primary CPU switching to normal world boot
I/TC: Reserved shared memory is disabled
I/TC: Dynamic shared memory is enabled
I/TC: Normal World virtualization support is disabled
I/TC: Asynchronous notifications are disabled
optee optee: OP-TEE: revision 4.0 (2a5b1d12)
serial_stm32 serial@40010000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19
U-Boot 2023.10-stm32mp-r1 (Oct 02 2023 - 14:39:59 +0000)
CPU: STM32MP151CAA Rev.Z
Model: STMicroelectronics custom STM32CubeMX board - openstlinux-6.6-yocto-scarthgap-mpu-v25.06.11
Board: stm32mp1 in trusted mode (st,stm32mp151c-chargehub-mx)
DRAM: no /fwu-mdata node ?
512 MiB
optee optee: OP-TEE: revision 4.0 (2a5b1d12)
I/TC: Reserved shared memory is disabled
I/TC: Dynamic shared memory is enabled
I/TC: Normal World virtualization support is disabled
I/TC: Asynchronous notifications are disabled
Clocks:
- MPU : 650 MHz
- MCU : 200 MHz
- AXI : 233 MHz
- PER : 24 MHz
- DDR : 466 MHz
Core: 113 devices, 33 uclasses, devicetree: board
WDT: Started watchdog with servicing every 1000ms (32s timeout)
NAND: 0 MiB
MMC: STM32 SD/MMC: 0, STM32 SD/MMC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
invalid MAC address 0 in OTP 00:00:00:00:00:00
Net:
Error: ethernet@5800a000 address not set.
No ethernet found.
After a few seconds, I have a
No Ethernet found is the last message in the log. I think the problem is not the Ethernet. How to resolve this problem?
I use the latest OpenStLinux. In the attachment, I added U-Boot DTS.
Additionally, I can't stop the U-Boot by pressing any key.
Thanks for any help
BR Michal
2025-07-19 9:03 AM
It is very strange. I removed SDMMC2, and the system starts boots. In my opinion, even if SDMMC2 is not working or not soldered, it should go. Do I miss some option during system customisation?
2025-07-20 4:07 PM
Hello,
The same applies to NAND Flash. If I activate it in U-Boot DTS, it gets stuck on "NAND: ". That's all, the watchdog resets it. Why does U-Boot get stuck? How can I check what happened? NAND flash and EMMC are empty.
BR Michal
2025-07-23 9:56 AM - edited 2025-07-23 9:57 AM
I have a bit of confirmation about my theory, checked on good hardware. When the EMMC is bad solder or bad hardware design, it gets stuck on U-Boot as above. I think the same probably is with the NAND.
Can someone confirm this theory?
BR
Michal