2025-02-21 01:09 AM
Hi, I am using STM32MP2157F-DK microcontroller. I have never used a dual cortex before. All I want to do is to generate a simple STM32CubeIDE project which also has a .ioc file. I want to debug it via CubeIDE.
1) Do I need OpenAmp to successfully flash the code?
2) I have already set up the SDK, are there other settings I need to take care of?
When I try to flash my current project, It always stops at 78% like shown in the picture below.