cancel
Showing results for 
Search instead for 
Did you mean: 

How to create STM32MP157AAAx Example Project

MBhin
Associate III

Hi ST Community,

i am using STM32CubeIDE. But i can not create an example project as i am getting the following error.

0690X000008iVU1QAM.jpg

But according to old posts related to STM32MP157, other users have created the example project successfully. Need some help please for getting started.

i am using STM32CubeIDE v1.0.0.

Best Regards,

Usman

21 REPLIES 21

Thanks @MBhin​  for your feedback.

Can we conclude that problem in post https://community.st.com/s/question/0D50X0000B2ATz4SQG/stm32mp157xeval-populate-the-target-and-boot-the-image-related-issue was the same and is also non longer active ?

If yes would you mind to enter a comment to close the discussion ?

BR,

Thx

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MBhin
Associate III

@Community member​  yes it was also the same.

Best Regards,

Usman