cancel
Showing results for 
Search instead for 
Did you mean: 

Does the STM32CubeIDE 1.0.2 ( windows 10) support STM32MP157?

aman.32
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Olivier GALLIEN
ST Employee

Hi @aman.32​ 

Yes STM32CubeIDE V1.1.0 supporting MP1 is about to be available on st.com along with the new V1.1.0 STM32MP15 ecosystem release.

Refer to Release note and stay tune

https://wiki.st.com/stm32mpu/index.php/STM32MP15_ecosystem_release_note

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
victor.b
Associate II

Not yet, I belive it will soon support it.

In the meanwhile there is the famous and broken SW4STM32 or there is Keil, witch i switched to and it works flawlessly.

aman.32
Associate II

Thank you. My current Keil uVision is 5.24.2. Do I need to update the software?

PFran.17
Associate II

Hi,

in October 2019 is not still supported. Is there any update scheduled soon?

Olivier GALLIEN
ST Employee

Hi @aman.32​ 

Yes STM32CubeIDE V1.1.0 supporting MP1 is about to be available on st.com along with the new V1.1.0 STM32MP15 ecosystem release.

Refer to Release note and stay tune

https://wiki.st.com/stm32mpu/index.php/STM32MP15_ecosystem_release_note

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.