2022-01-20 04:38 AM
2022-01-20 06:45 AM
2022-01-20 06:45 AM
Solved.
I had to enable the APB4 clock (0x50000200 = 0x8000).
2022-01-20 07:23 AM
Hello @42Bastian Schick ,
Yes, you found it. Thanks for coming back to post the solution :).
As explained page 584 in the Reference Manual RM0436 rev5.0: https://www.st.com/resource/en/reference_manual/DM00327659-.pdf
The APB4 clock is needed to access to the IWDGx registers of IWDG2.
Regards,
Kévin
2022-01-20 07:28 AM
The confusion came because the registers could be read. Most often, if the clock is not enabled, you cannot even read the registers.
Cheers
42Bastian