2023-05-09 6:41 AM
Hi,
I am confused how to correctly set u-boot environment variables in a system based on OpenST Linux 4.1 and follows DK2 settings.
The partition layout looks like this:
#Opt Id Name Type IP Offset Binary
- 0x01 fsbl1-boot Binary none 0x0 arm-trusted-firmware/tf-a-stm32mp157f-nexio-usb.stm32
- 0x03 fip-boot Binary none 0x0 fip/fip-stm32mp157f-nexio-trusted.bin
P 0x04 fsbl1 Binary mmc0 0x00004400 arm-trusted-firmware/tf-a-stm32mp157f-nexio-sdcard.stm32
P 0x05 fsbl2 Binary mmc0 0x00044400 arm-trusted-firmware/tf-a-stm32mp157f-nexio-sdcard.stm32
P 0x06 metadata1 Binary mmc0 0x00084400 arm-trusted-firmware/metadata.bin
P 0x07 metadata2 Binary mmc0 0x000C4400 arm-trusted-firmware/metadata.bin
P 0x08 fip-a FIP mmc0 0x00104400 fip/fip-stm32mp157f-nexio-trusted.bin
PED 0x09 fip-b FIP mmc0 0x00504400 none
PED 0x0A u-boot-env Binary mmc0 0x00904400 none
P 0x10 bootfs System mmc0 0x00984400 st-image-bootfs-openstlinux-weston-stm32mp1-nexio.ext4
P 0x11 vendorfs FileSystem mmc0 0x04984400 st-image-vendorfs-openstlinux-weston-stm32mp1-nexio.ext4
P 0x12 rootfs FileSystem mmc0 0x05984400 st-image-core-openstlinux-weston-stm32mp1-nexio.ext4
P 0x13 rootfs FileSystem mmc0 0x45984400 st-image-core-openstlinux-weston-stm32mp1-nexio.ext4
E 0x14 writeable FileSystem mmc0 0x85984400 none # 256kB persistent memory
E 0x15 dummy FileSystem mmc0 0x859C4400 none # unused
My idea is to use u-boot boot.scr.cmd to be able to switch between the two root filesystems.
fw_env.config looks like this:
# Block device example
/dev/disk/by-partlabel/u-boot-env 0x3bc00 0x2000
/dev/disk/by-partlabel/u-boot-env 0x3bc00 0x2000
I got the start offset by looking into u-boot-env by using hexdump.
After boot I am able to use fw_printenv and fw_setenv and I see the changes made to u-boot-env.
But I have a number of issues with this approach:
How can I configure the system so that u-boot and the rootfs use the same device for storing the FW environment variables?
Thank you 1000 times!
bye Gunther
Solved! Go to Solution.
2023-05-09 7:41 AM
I believe I found the culprit;
Somehow our u-boot device tree set:
u-boot,mmc-env-partition = "fip";
I am changing it to:
u-boot,mmc-env-partition = "u-boot-env";
and expecting consistent behavior.
Bye Gunther
2023-05-09 7:41 AM
I believe I found the culprit;
Somehow our u-boot device tree set:
u-boot,mmc-env-partition = "fip";
I am changing it to:
u-boot,mmc-env-partition = "u-boot-env";
and expecting consistent behavior.
Bye Gunther
2023-06-19 4:58 AM
Hi,
I confirm, that is a modification in U-Boot device tree on ST boards for OpenSTLinux migration V3.X => V4.X to respect the new flashlayout = https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#SD_card
A new partition is created for save the U-Boot environment, it is no more saved at the end of the FIP partition.
If you can adopt the new SD-Card partitioning (the new tsv files) you must update this part in your U-Boot device tree:
https://wiki.st.com/stm32mpu/wiki/U-Boot_overview#U-Boot_environment_variables
sorry if it was clear enough.
Patrick