2020-05-19 12:43 AM
Is there any application note for tamper pins? Which one of the pins is the active tamper?
2020-05-19 1:20 AM
Hello,
Active Tamper need a couple of pins, TAMP_OUT and TAMP_IN, connected on PCB by various security mechanism (wires, mesh, switch, sensors, etc..).
Examples of connections are:
or
or
or
Regards
2020-08-09 6:47 AM
Hi Patrick,
I'm using the 257 pins package of the STM32MP153 with Ethernet.
So PC1 is used for ETH_MDC.
PI8 is not available because of the package.
Does this means I can't use active tamper?
Regards,
Ofer