2019-11-21 10:41 PM
For STPMIC1, when it is powered on by asserting the PONKEYn signal low, what would happen if the PONKEYn remains asserted low even after the initial POWER_ON trigger? Would it subsequently trigger a POWER_DOWN if PONKEYn long press turn off is activated? Or is the PONKEYn event triggered only when there is a HIGH to LOW edge transition (edge trigger) ?
Thanks.
Steven
Solved! Go to Solution.
2019-11-26 05:36 AM
Hi @SYEH
In that case STPMIC1 will not trig a POWER DOWN. You need another HIGH to LOW edge transition to start the Long Key Press timer.
Hope it help,
Olivier
2019-11-26 05:36 AM
Hi @SYEH
In that case STPMIC1 will not trig a POWER DOWN. You need another HIGH to LOW edge transition to start the Long Key Press timer.
Hope it help,
Olivier
2019-11-26 06:17 AM
Hi Olivier,
Thanks for the reply. Understood.
Is that the same for the WAKEUP pin? As in the WAKEUP POWER_ON event will only trigger from LOW to HIGH edge transition, and does not require to stay HIGH after the initial trigger?
Thanks.
Steven.
2019-11-26 06:44 AM
Yes WAKEUP pin is edge sensitive. Except in the situation explain in DataSheet Figure 58. Turn-on condition before VIN_POR_Rise.
Olivier
2019-12-02 11:13 PM
Hi Olivier,
Thanks for the response. Much appreciated.
All clear now.
Cheers.
Steven