cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP15x: NRST doesn't work after login prompt occurs

Dat Tran
Senior II

Hi,

We are working on STM32MP151, with custom linux, no PMIC.

We have a reset button connect to NRST line, it works fine in Uboot or during linux boots. But right after the login prompt occurs, the reset button is nolonger work. When we hit the button, system seems crashed, no response from command prompt. We have to disconnect power and reconnect again.

Does anyone have experience with it?

many thanks.

1 ACCEPTED SOLUTION

Accepted Solutions
PatrickF
ST Employee

Hi @Community member​ 

If your solution does not use STPMIC1, there is a Limitation which could be the root cause of your issue.

Please have a look to ES0438: 2.3.5 Incorrect reset of glitch-free kernel clock switch

See also AN5031 which show the recommended HW if your power solution does not make a power cycle upon NRST activation.


_legacyfs_online_stmicro_images_0693W00000bk63fQAA.pngRegards

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Dat Tran
Senior II

is there any idea please?

PatrickF
ST Employee

Hi @Community member​ 

If your solution does not use STPMIC1, there is a Limitation which could be the root cause of your issue.

Please have a look to ES0438: 2.3.5 Incorrect reset of glitch-free kernel clock switch

See also AN5031 which show the recommended HW if your power solution does not make a power cycle upon NRST activation.


_legacyfs_online_stmicro_images_0693W00000bk63fQAA.pngRegards

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Dat Tran
Senior II

Thank you so much, we will take a look at let you know.

Dat Tran
Senior II

Hi @PatrickF​ , we changed our module as your suggestion and the reset button works perfectly.

Thank you so much for the information.