cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157F: DMA support on USB/CRYPTO/eMMC

ALong.4
Associate II

Hi,

I am interested in using the STM32MP157F for the following tasks:

  1. Receiving data from USB 2.0.
  2. Encrypting the received data using AES 256.
  3. Storing the encrypted data in an external eMMC.
  4. Preferably utilizing DMA for efficient data transfers.

I would like to know if it is possible to configure DMA channels to enable direct peripheral-to-peripheral communication, such as USB 2.0 -> CRYPTO (AES 256) -> eMMC.

Additionally, it would be greatly appreciated if you could provide an example or reference on how to utilize DMA with USB, cryptographic operations, and eMMC.

Thank you.

Best regards,

Alessandro

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0