2025-05-02 8:51 AM
Hi,
We are working on a custom carrier board based on STM32MP157DAC. We have built a custom yocto image.
I have attached the dmesg log and device tree configuration.
Is the driver support for this wifi-bt module directly available or do I need to configure something?
bluetooth is configured as serial3 but I don't see any /dev/ttySTM2 device node.
[ 14.597018] Bluetooth: Core ver 2.22
[ 14.606728] Bluetooth: HCI device and connection manager initialized
[ 14.614038] Bluetooth: HCI socket layer initialized
[ 14.629270] Bluetooth: L2CAP socket layer initialized
[ 14.637891] Bluetooth: SCO socket layer initialized
[ 14.658379] Bluetooth: HCI UART driver ver 2.3
[ 14.669248] Bluetooth: HCI UART protocol H4 registered
[ 14.675392] Bluetooth: HCI UART protocol Broadcom registered
[ 14.986555] Bluetooth: hci0: Frame reassembly failed (-84)
[ 15.485933] Bluetooth: hci0: Frame reassembly failed (-84)
[ 15.985947] Bluetooth: hci0: Frame reassembly failed (-84)
[ 16.485928] Bluetooth: hci0: Frame reassembly failed (-84)
[ 16.985992] Bluetooth: hci0: Frame reassembly failed (-84)
[ 17.110864] Bluetooth: hci0: command 0xfc18 tx timeout
[ 25.430835] Bluetooth: hci0: BCM: failed to write update baudrate (-110)
[ 25.436194] Bluetooth: hci0: Failed to set baudrate
[ 25.485997] Bluetooth: hci0: Frame reassembly failed (-84)
[ 25.986019] Bluetooth: hci0: Frame reassembly failed (-84)
I am getting above error regarding bluetooth but i dont see any logs regarding wifi in dmesg.
Thanks