2025-01-12 11:10 AM - edited 2025-01-12 11:24 AM
Hello,
I am running a Linux image based on meta-st-stm32mp (hardknott branch).
I currently have the following in my host device tree:
reserved-memory {
#address-cells = <1>;
#size-cells = <1>;
ranges;
mcuram2: mcuram2@10000000 {
compatible = "shared-dma-pool";
reg = <0x10000000 0x40000>;
no-map;
};
vdev0vring0: vdev0vring0@10040000 {
compatible = "shared-dma-pool";
reg = <0x10040000 0x1000>;
no-map;
};
vdev0vring1: vdev0vring1@10041000 {
compatible = "shared-dma-pool";
reg = <0x10041000 0x1000>;
no-map;
};
vdev0buffer: vdev0buffer@10042000 {
compatible = "shared-dma-pool";
reg = <0x10042000 0x4000>;
no-map;
};
mcuram: mcuram@30000000 {
compatible = "shared-dma-pool";
reg = <0x30000000 0x40000>;
no-map;
};
retram: retram@38000000 {
compatible = "shared-dma-pool";
reg = <0x38000000 0x10000>;
no-map;
};
gpu_reserved: gpu@d4000000 {
reg = <0xd4000000 0x4000000>;
no-map;
};
};
mlahb: ahb {
compatible = "st,mlahb", "simple-bus";
#address-cells = <1>;
#size-cells = <1>;
ranges;
dma-ranges = <0x00000000 0x38000000 0x10000>,
<0x10000000 0x10000000 0x60000>,
<0x30000000 0x30000000 0x60000>;
m4_rproc: m4@10000000 {
compatible = "st,stm32mp1-m4";
reg = <0x10000000 0x40000>,
<0x30000000 0x40000>,
<0x38000000 0x10000>;
/* ... */
};
};
mlahb is from the stm32mp151.dtsi.
Let's say, we'd like to increase the allowed image size to 128kb by changing 0x10000 to 0x20000:
&retram {
reg = <0x38000000 0x20000>;
};
&mlahb {
dma-ranges = <0x00000000 0x38000000 0x20000>,
<0x10000000 0x10000000 0x60000>,
<0x30000000 0x30000000 0x60000>;
m4_rproc {
reg = <0x10000000 0x40000>,
<0x30000000 0x40000>,
<0x38000000 0x20000>;
};
};
Unfortunately, when trying to load a firmware (echo start > /sys/class/remoteproc/remoteproc0/state),
I still get a kernel crash:
[ 376.591779] 8<--- cut here ---
[ 376.593848] Unhandled fault: imprecise external abort (0x1c06) at 0x004627a4
[ 376.600885] pgd = fc518049
[ 376.603571] [004627a4] *pgd=c5ef0835, *pte=00000000, *ppte=00000000
[ 376.609836] Internal error: : 1c06 [#1] PREEMPT SMP ARM
[ 376.615042] Modules linked in: rpmsg_tty rpmsg_core etnaviv gpu_sched spi_stm32 stm32_rproc sch_fq_codel ipv6
[ 376.624955] CPU: 1 PID: 298 Comm: sh Not tainted 5.10.10 #1
[ 376.630507] Hardware name: STM32 (Device Tree Support)
[ 376.635648] PC is at memcpy+0x54/0x330
[ 376.639374] LR is at 0x6263000a
[ 376.642499] pc : [<c060d914>] lr : [<6263000a>] psr: 20000013
[ 376.648753] sp : c5cfbe2c ip : 2172656c fp : e0d20000
[ 376.653965] r10: 00000000 r9 : 00000000 r8 : 646e6168
[ 376.659180] r7 : 206b6361 r6 : 626c6c61 r5 : 63206f4e r4 : 09007265
[ 376.665696] r3 : 6c646e61 r2 : 000011b4 r1 : e0bc9220 r0 : e0d30120
[ 376.672213] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment none
[ 376.679336] Control: 10c5387d Table: c5ea006a DAC: 00000051
[ 376.685072] Process sh (pid: 298, stack limit = 0x86cbec92)
[ 376.690629] Stack: (0xc5cfbe2c to 0xc5cfc000)
[ 376.694979] be20: 00011354 00011354 00000001 00000000 e0d20000
[ 376.703147] be40: e0bb9054 c0a0a584 00011354 10041000 00000000 00000000 00000000 c01175f4
[ 376.711314] be60: 00000100 00000000 00000006 00000001 00000020 c34cd800 c5ea7cc0 c121f270
[ 376.719482] be80: e0bb9000 c34cd820 c0a06c88 c34cd800 c34cd800 c34cd820 c5ea7cc0 c35c2840
[ 376.727649] bea0: 00000000 00000000 00000000 c0be8e54 00000000 c34cd800 c5ea7cc0 c34cd820
[ 376.735817] bec0: c35c2840 c0be9380 c34cd800 c34cd9e8 00000000 c34cd9f4 c34cd820 c0a07f78
[ 376.743984] bee0: c5ea7cc0 3a12e441 00000cc0 c34cd820 c5ea7a80 00000006 c34cd800 c5ea6610
[ 376.752151] bf00: 00000051 c0a097bc 00000006 c5ea6600 c5ea7a80 c5cfbf80 c5ea6610 c03a3c48
[ 376.760317] bf20: 00000000 00000000 0000000b c3337c00 00000006 c03a3b50 00534fb0 c5cfbf80
[ 376.768484] bf40: c2de3c00 00000004 0052f2f0 c0302348 c316d900 3a12e441 c316d900 00000000
[ 376.776650] bf60: c1894900 c3337c00 c3337c00 00000000 00000000 c0100264 c5cfa000 c03026e8
[ 376.784816] bf80: 00000000 00000000 c5cfa000 3a12e441 00000003 00000006 00534fb0 b6f6c1e0
[ 376.792984] bfa0: 00000004 c0100060 00000006 00534fb0 00000001 00534fb0 00000006 00000000
[ 376.801152] bfc0: 00000006 00534fb0 b6f6c1e0 00000004 00000000 bee1b7f0 00534fb0 0052f2f0
[ 376.809318] bfe0: 00000004 bee1b7a0 b6e7135f b6dfd386 60000030 00000001 00000000 00000000
[ 376.817517] [<c060d914>] (memcpy) from [<c0a0a584>] (rproc_elf_load_segments+0x1a0/0x288)
[ 376.825669] [<c0a0a584>] (rproc_elf_load_segments) from [<c0be8e54>] (rproc_start+0x24/0x154)
[ 376.834171] [<c0be8e54>] (rproc_start) from [<c0be9380>] (rproc_fw_boot+0x170/0x1a4)
[ 376.841898] [<c0be9380>] (rproc_fw_boot) from [<c0a07f78>] (rproc_boot+0x150/0x1a4)
[ 376.849541] [<c0a07f78>] (rproc_boot) from [<c0a097bc>] (state_store+0x40/0xc8)
[ 376.856841] [<c0a097bc>] (state_store) from [<c03a3c48>] (kernfs_fop_write+0xf8/0x21c)
[ 376.864750] [<c03a3c48>] (kernfs_fop_write) from [<c0302348>] (vfs_write+0xc0/0x318)
[ 376.872481] [<c0302348>] (vfs_write) from [<c03026e8>] (ksys_write+0x60/0xe4)
[ 376.879603] [<c03026e8>] (ksys_write) from [<c0100060>] (ret_fast_syscall+0x0/0x54)
[ 376.887237] Exception stack(0xc5cfbfa8 to 0xc5cfbff0)
[ 376.892282] bfa0: 00000006 00534fb0 00000001 00534fb0 00000006 00000000
[ 376.900451] bfc0: 00000006 00534fb0 b6f6c1e0 00000004 00000000 bee1b7f0 00534fb0 0052f2f0
[ 376.908613] bfe0: 00000004 bee1b7a0 b6e7135f b6dfd386
[ 376.913659] Code: f5d1f07c e8b151f8 e2522020 e8a051f8 (aafffffa)
[ 376.919737] ---[ end trace e8ef0d82ecc3eec4 ]---
[ 376.925593] 8<--- cut here ---
[ 376.927384] Unhandled fault: imprecise external abort (0x1c06) at 0x004627a4
[ 376.934422] pgd = 6e154e4d
[ 376.937107] [004627a4] *pgd=c5c11835, *pte=00000000, *ppte=00000000
This only happens if the actual firmware image has a code+data section larger than 64kb.
Does anybody have any clue what I am missing in the device tree?
I should also try to get a proper backtrace of that crash...
What's the hard limit for M4 firmwares?
In this comment, @PatrickF said that it's at most 448kb:
https://community.st.com/t5/stm32-mpus-products/possible-advisable-to-increase-the-size-of-m4-coprocessor-text/m-p/51879/highlight/true#M52
What's colliding with the RETRAM section or is it because the M4 core won't execute directly from
RETRAM, but copies code into one of the mcuram regions?
See https://wiki.st.com/stm32mpu/wiki/STM32MP15_MCU_SRAM_internal_memory
Is it the mcuram region that I have to increase?
Yours sincerely,
Robin Haberkorn
2025-01-27 07:08 AM
Do you also update the "vdev0XXXX" memory regions accordingly in the Linux Device tree?
https://elixir.bootlin.com/linux/v6.13-rc3/source/arch/arm/boot/dts/st/stm32mp15xx-dkx.dtsi#L22
2025-01-29 12:41 PM
@ArnaudP wrote:Do you also update the "vdev0XXXX" memory regions accordingly in the Linux Device tree?
https://elixir.bootlin.com/linux/v6.13-rc3/source/arch/arm/boot/dts/st/stm32mp15xx-dkx.dtsi#L22
Yes, of course. For instance I tried these adaptions on top of the default memory layout (which I summarized at the very beginning of this thread):
reserved-memory { mcuram3: mcuram3@10020000 { compatible = "shared-dma-pool"; reg = <0x10020000 0x3A000>; no-map; }; /delete-node/vdev0vring0; vdev0vring0@1005A000 { compatible = "shared-dma-pool"; reg = <0x1005A000 0x1000>; no-map; }; /delete-node/vdev0vring1; vdev0vring1@1005B000 { compatible = "shared-dma-pool"; reg = <0x1005B000 0x1000>; no-map; }; /delete-node/vdev0buffer; vdev0buffer@1005C000 { compatible = "shared-dma-pool"; reg = <0x1005C000 0x4000>; no-map; }; }; }; &mcuram2 { reg = <0x10000000 0x20000>; }; &m4_rproc { memory-region = <&retram>, <&mcuram>, <&mcuram2>, <&mcuram3>, <&vdev0vring0>, <&vdev0vring1>, <&vdev0buffer>; /* Why are the vdev0ringX sections missing in this node? */ reg = <0x10000000 0x20000>, /* mcuram2 */ <0x10020000 0x3A000>, /* mcuram3 */ <0x30000000 0x40000>, /* mcuram (???) */ <0x38000000 0x10000>; /* retram */ m4_system_resources { status = "okay"; }; };
I had analogous declarations in the Zephyr device tree:
zephyr,ipc_shm = &mcuram4; /* ... */ mcuram4: memory4@1005A000 { compatible = "mmio-sram"; reg = <0x1005A000 0x6000>; };
But unfortunately, I could not get rpmsg_create_ept() to initialize with these settings. I didn't do any further debugging as this reshuffling of memory sections wasn't strictly necessary for what I was trying to achieve - I just declared a third code section at 0x10046000 without moving the IPC buffers from their default location.