2019-07-18 6:11 AM
I've tried to flash STM32MP157C-DK2 SDCard like described in ST wiki with command STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsv.
and it didn't work! i got following error report. it seems it has trouble to reconnect the device. does anyone have an idea why it didn't work? or does anybody get similar problem? how do i get it working? Thanks a lot!
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
SN : 0036004A3338510939303435
FW version : 0x0110
Device ID : 0x0500
Device name : STM32MPxxx
Device type : MPU
Device CPU : Cortex-A7
Start Embedded Flashing service
Memory Programming ...
Opening and parsing file: tf-a-stm32mp157c-dk2-trusted.stm32
File : tf-a-stm32mp157c-dk2-trusted.stm32
Size : 245360 Bytes
Partition ID : 0x01
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:04.627
RUNNING Program ...
PartID: :0x01
Start operation done successfully at partition 0x01
Flashlayout Programming ...
[==================================================] 100%
Running Flashlayout Partition ...
Flashlayout partition started successfully
Memory Programming ...
Opening and parsing file: u-boot-stm32mp157c-dk2-trusted.stm32
File : u-boot-stm32mp157c-dk2-trusted.stm32
Size : 748660 Bytes
Partition ID : 0x03
Download in Progress:
[==================================================] 100%
File download complete
Time elapsed during download operation: 00:00:13.495
RUNNING Program ...
PartID: :0x03
reconnecting the device ...
Error: unable to reconnect the target device: time out expired
Error: Start operation failed at partition 0x03
Error: TSV flashing service failed
2019-07-18 7:05 AM
could that be an issue with power? i power it first not with 3A supply.
2019-07-18 7:09 AM
You are using an USB Full-Speed port (12Mbits/s), maybe this is the problem, could you try to add -tm 20000 to the CubeProgrammer command line ?
Could you also log the console output (available as VCP 115200 8 N 1 using ST-Link connector) ?
could you provide DK2 serial number (available on a white sticker on the backside of the PCB) ?
2019-07-18 7:43 AM
no! i tried it with -tm command. it didn't work. same result like before.
and console output is:
partittions : Writing GPT : success!
done
DFU alt info setting: done
crq -> brequest: 0x0
i believe DK2 serial number: DK32MP157C2$AU1
2019-07-18 8:37 AM
Maybe an issue with DFU driver (reconnect is using a different DFU descriptor), please have a look to https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer#Preparing_the_USB_serial_link_for_flashing
2019-07-19 12:33 AM
I've already done that! That doesn't help.
2019-07-19 4:01 AM
Hi! Patrick,
can this issue be power supply issue? because i still use a 2.1A supply and the LED is still red. is it that means that the device can not boot itself successfully? i order a 3A supply and hope it will work and besides can i boot the system and flash the image per other memory medium than SD card? i search the board documentation but no found SPI or QSPI memory medium, is it still other way or any other sample software i can follow? Thank you very much!
2019-07-19 6:14 AM
If you supply is stated 2.1A, I think this is not the root cause of your problem. The red toggling led is because the supply is not detected as a true 5V 3A USB Type-C supply.
I'm puzzled by the "Full Speed (12MBit/s)" message which mean your PC might have some strange set-up.
Btw, in the UART4 console message (Virtual Comm Port available when you connect the ST-Link cable), you should have much more messages than you copied above. Could you please log all in a file ?
Did you set the DK2 dip switches in the right position for Flash load ? see https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157C-DK2/Let%27s_start/Populate_the_target_and_boot_the_image
Last solution, if you have a Linux PC (or a Virtual Machine running Ubuntu, see https://wiki.st.com/stm32mpu/wiki/PC_prerequisites), you could program the SD-Card outside DK2, directly on a PC using for example an USB->micro-SD adapter. see https://wiki.st.com/stm32mpu/wiki/How_to_populate_the_SD_card_with_dd_command
2019-07-22 6:29 AM
so i acceeded to create the image file with shell file and flashed it with SD adapter. It worked. but i still struggle how i can flash it with the hardware! for log message I'll get some more!
2019-07-22 7:13 AM
i mean succeeded