cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32mp157a kernal booting issue

Sindhu Vadde
Associate III

Hi,

We are using stm32mp157a processor in my custom board.I have download stm32mp157a-dk1 discovery kit code.The difference between discovery board and my custom board is Debug Serial port Configuration.

In Discovery Board The debug uart pins are

PG11-->UART4_TX

PB2-->UART4_RX.

where as in my custom board the pins are different

PE0--> UART8_TX

PE1-->UART8_RX

So I have changed the pin muxing and nodes in dts files. And debug_uart_init() in Uboot source code. Up to Uboot It is working fine. I have done the same configuartion except debug_uart_init() in kernal source code.why because debug_uart_init() function is not there in linux source code. when can i get kernal log in my custom board. Please help me in this regards. You can see my log below.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

Hi @Sindhu Vadde​ ,

seems there is other difference, please check pins PA13 and PA13 as it seems you have activated USB boot with this pins (so kernel is not started).

See https://wiki.st.com/stm32mpu/wiki/How_to_configure_U-Boot_for_your_board#Config_node

especially st,stm32prog-gpios definition

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.