cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32mp157a Emmc Booting Issue in Custom board?

Sindhu Vadde
Associate III

Hi,

I am using stm32mp157a processor in my custom board. Fsbl and ssbl is booting from Sd card.When i try boot through Emmc it is not working,even files are not loading. I have followed below link for emmc booting https://community.st.com/s/question/0D53W00000HypghSAB/emmc-questions

When i enter ext4load mmc 0:4 0xC0000000 tf-a-stm32mp157a-dk1.stm32 command in u boot prompt it is showing below Error.

Failed to load tf-a-stm32mp157a-dk1.stm32. What is the issue.How can i resolve this error.

2 REPLIES 2
PatrickF
ST Employee

Hi @Sindhu Vadde​,

Could you share more information on your overall HW setup ?

  • Did you use default eMMC boot pins (as stated in AN5031 or (https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_code_overview#Boot_from_e-E2-80-A2MMC-E2-84-A2) ? Otherwise, did you setup OTPs?
  • Could you share the BootROM log (https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ROM_trace_analyzer#On_STM32MP15x_lines) ?
  • Please confirm you are using a Silicon Rev.Z ? Rev.B has boot issue with most eMMC (See ES0438 for details)
  • Did you try programming eMMC using USB with CubeProgrammer ?

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
PatrickF
ST Employee

Hi @Sindhu Vadde​ 

did you progress on this issue ?

Regards.

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.