2019-12-06 11:35 PM
I used the i2c4 for sii9022 chip,but it always busy and don't response for hdmi plug in.
2019-12-09 02:19 AM
I2C bus busy is usually a bus stuck to 0V, e.g. wrong Hw connection or missing power supplies on one of the I2C slave device on the bus (devices are not always "fail-safe" on their I2C pins)
2019-12-09 02:29 AM
No, it actually works, only to detect the bus reusable by I2C4 will time out
and my i2c4 dts and sch,can you help me,i spend three days but no result...:loudly_crying_face: :loudly_crying_face: :loudly_crying_face:
2019-12-09 02:31 AM
and i don't know the 9022 chip always busy,disabled the hdmi always ok.
2019-12-09 02:41 AM
From HW point if view, I just see that CI2CA pull-down should be 4.7k whereas you have 10k. Not sure it will be the issue, but deserve to align with Si9022 datasheet value.
For SW or DT settings, I cannot help much.
2019-12-09 05:28 AM
My dts is ok?
2020-04-02 10:42 PM
hi:
2020-04-13 07:38 AM
Yes
2020-04-13 07:39 AM
Using another esd chip or set pull up res to dscl and dsda:|
2020-04-13 07:41 AM
Sorry.NO,I guess this is a bug...