cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP1 ethernet issue

stefboerrigter
Associate II

Hi,

We are using the STM32MP157CAA3 SoC in our design and are having some Ethernet issues:

As we had problems sourcing the Realtek PHY from the reference design we use the microchip LAN8830T-V/PSA Ethernet PHY which should support Gigabit Ethernet.
When setting booting the device and connecting an Ethernet cable we observe the following issue:
1. With 10 MBit or router, the device probes and from both U-boot and Linux we can do dhcp request. But we never get an answer (no IP etc). 
2. With 100 MBit or 1000 MBit speed, the linux kernel throws a panic after some time related to DMA (sometimes also the probing fails for the DMA engine).

Both paths never show any data coming through the Ethernet port:  (DCHP requests seem to be unanswered (don't arrive on server side) and ping also doesn't arrive. LED's remain stale (green = constant ON, orange LED = off). 

Bootlog during success:

root@board:~# dmesg | grep eth
[ 0.000000] psci: probing for conduit method from DT.
[ 0.269703] usbcore: registered new interface driver cdc_ether
[ 0.289476] optee: probing for conduit method.
[ 1.633140] stm32-dwmac 5800a000.ethernet: IRQ eth_lpi not found
[ 1.638473] stm32-dwmac 5800a000.ethernet: no regulator found
[ 1.638983] stm32-dwmac 5800a000.ethernet: User ID: 0x40, Synopsys ID: 0x42
[ 1.644693] stm32-dwmac 5800a000.ethernet: DWMAC4/5
[ 1.649759] stm32-dwmac 5800a000.ethernet: DMA HW capability register supported
[ 1.656999] stm32-dwmac 5800a000.ethernet: RX Checksum Offload Engine supported
[ 1.664289] stm32-dwmac 5800a000.ethernet: TX Checksum insertion supported
[ 1.671191] stm32-dwmac 5800a000.ethernet: Wake-Up On Lan supported
[ 1.677637] stm32-dwmac 5800a000.ethernet: TSO supported
[ 1.682709] stm32-dwmac 5800a000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 1.690628] stm32-dwmac 5800a000.ethernet: Enabled L3L4 Flow TC (entries=2)
[ 1.697535] stm32-dwmac 5800a000.ethernet: Enabled RFS Flow TC (entries=10)
[ 1.704522] stm32-dwmac 5800a000.ethernet: TSO feature enabled
[ 1.710332] stm32-dwmac 5800a000.ethernet: Using 32/32 bits DMA host/device width
[ 4.623237] stm32-dwmac 5800a000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 4.631424] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [Generic PHY] (irq=POLL)
[ 4.644235] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 4.651974] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 4.660496] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[ 4.668620] stm32-dwmac 5800a000.ethernet eth0: configuring for phy/rgmii-id link mode
[ 8.880230] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 10Mbps/Full - flow control rx/tx
[ 8.887340] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

Bootlog during failure:

root@wesl:~# dmesg | grep eth
[ 0.000000] psci: probing for conduit method from DT.
[ 0.269963] usbcore: registered new interface driver cdc_ether
[ 0.289696] optee: probing for conduit method.
[ 1.633444] stm32-dwmac 5800a000.ethernet: IRQ eth_lpi not found
[ 1.638790] stm32-dwmac 5800a000.ethernet: no regulator found
[ 1.639302] stm32-dwmac 5800a000.ethernet: User ID: 0x40, Synopsys ID: 0x42
[ 1.645012] stm32-dwmac 5800a000.ethernet: DWMAC4/5
[ 1.650074] stm32-dwmac 5800a000.ethernet: DMA HW capability register supported
[ 1.657319] stm32-dwmac 5800a000.ethernet: RX Checksum Offload Engine supported
[ 1.664610] stm32-dwmac 5800a000.ethernet: TX Checksum insertion supported
[ 1.671509] stm32-dwmac 5800a000.ethernet: Wake-Up On Lan supported
[ 1.677850] stm32-dwmac 5800a000.ethernet: TSO supported
[ 1.683023] stm32-dwmac 5800a000.ethernet: Enable RX Mitigation via HW Watchdog Timer
[ 1.690841] stm32-dwmac 5800a000.ethernet: Enabled L3L4 Flow TC (entries=2)
[ 1.697848] stm32-dwmac 5800a000.ethernet: Enabled RFS Flow TC (entries=10)
[ 1.704736] stm32-dwmac 5800a000.ethernet: TSO feature enabled
[ 1.710643] stm32-dwmac 5800a000.ethernet: Using 32/32 bits DMA host/device width
[ 4.976410] stm32-dwmac 5800a000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 4.985026] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [Generic PHY] (irq=POLL)
[ 5.997554] stm32-dwmac 5800a000.ethernet: Failed to reset the dma
[ 6.002358] stm32-dwmac 5800a000.ethernet eth0: stmmac_hw_setup: DMA engine initialization failed
[ 6.011322] stm32-dwmac 5800a000.ethernet eth0: __stmmac_open: Hw setup failed
[ 9.224884] stm32-dwmac 5800a000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 9.241514] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [Generic PHY] (irq=POLL)
[ 9.254347] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 9.262215] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 9.271172] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[ 9.278538] stm32-dwmac 5800a000.ethernet eth0: configuring for phy/rgmii-id link mode
[ 13.439784] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 13.446896] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 19.687950] NETDEV WATCHDOG: eth0 (stm32-dwmac): transmit queue 0 timed out
[ 19.839844] stm32-dwmac 5800a000.ethernet eth0: Reset adapter.
[ 19.855494] stm32-dwmac 5800a000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 19.863823] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [Generic PHY] (irq=POLL)
[ 19.876709] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found
[ 19.884033] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported
[ 19.892921] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock
[ 19.898791] stm32-dwmac 5800a000.ethernet eth0: configuring for phy/rgmii-id link mode
[ 24.079787] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 24.086899] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

Panic:
[ 19.676490] ------------[ cut here ]------------
[ 19.679713] WARNING: CPU: 0 PID: 0 at net/sched/sch_generic.c:525 dev_watchdog+0x208/0x27c
[ 19.687950] NETDEV WATCHDOG: eth0 (stm32-dwmac): transmit queue 0 timed out
[ 19.694933] Modules linked in:
[ 19.697987] CPU: 0 PID: 0 Comm: swapper/0 Not tainted 6.1.28 #1
[ 19.703864] Hardware name: STM32 (Device Tree Support)
[ 19.709041] unwind_backtrace from show_stack+0x10/0x14
[ 19.714232] show_stack from dump_stack_lvl+0x40/0x4c
[ 19.719318] dump_stack_lvl from __warn+0x78/0x158
[ 19.724102] __warn from warn_slowpath_fmt+0x148/0x1c0
[ 19.729187] warn_slowpath_fmt from dev_watchdog+0x208/0x27c
[ 19.734882] dev_watchdog from call_timer_fn+0x34/0x1a8
[ 19.740079] call_timer_fn from __run_timers+0x274/0x378
[ 19.745370] __run_timers from run_timer_softirq+0x2c/0x40
[ 19.750863] run_timer_softirq from __do_softirq+0x138/0x408
[ 19.756555] __do_softirq from __irq_exit_rcu+0xc0/0x10c
[ 19.761837] __irq_exit_rcu from irq_exit+0x8/0x10
[ 19.766609] irq_exit from __irq_svc+0x88/0xc8
[ 19.771077] Exception stack(0xc1201ee8 to 0xc1201f30)
[ 19.776048] 1ee0: 00000000 00000000 0001c359 c0119740 00000000 c1208f40
[ 19.784247] 1f00: c1324320 c1208f40 00000000 00000000 10c5387d 00000000 7fffffff c1201f38
[ 19.792441] 1f20: c0109080 c0109084 60030013 ffffffff
[ 19.797504] __irq_svc from arch_cpu_idle+0x38/0x3c
[ 19.802287] arch_cpu_idle from default_idle_call+0x40/0x12c
[ 19.807977] default_idle_call from cpuidle_idle_call+0x18c/0x1ec
[ 19.814067] cpuidle_idle_call from do_idle+0x94/0xc8
[ 19.819145] do_idle from cpu_startup_entry+0x18/0x1c
[ 19.824122] cpu_startup_entry from rest_init+0xd0/0xd4
[ 19.829406] rest_init from arch_post_acpi_subsys_init+0x0/0x8
[ 19.835205] ---[ end trace 0000000000000000 ]---
[ 19.839844] stm32-dwmac 5800a000.ethernet eth0: Reset adapter.
[ 19.855494] stm32-dwmac 5800a000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0
[ 19.863823] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [Generic PHY] (irq=POLL)
[ 19.871457] dwmac4: Master AXI performs any burst length
[ 19.876709] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found

We have the idea that it is clock-tree related (See attached) .

The design is strapped so the PHY generates the clock-source (125MHz for 1GBit) 

Some matching issues that we searched on the forum: 

Relevant part of our schematics:Schematics.png

Our OPtee/tf-a rcc config see attached dts files (actually dtsi files, but not allowed). 
both are included by dts file like:

/dts-v1/;
#include "stm32mp157.dtsi"
#include "stm32mp15xc.dtsi"
#include "stm32mp15-pinctrl.dtsi"
#include "stm32mp15xxac-pinctrl.dtsi"
#include "stm32mp15xx-<ourBoard>-common.dtsi" //<-- the attached files
/ {

model = "proto 0 board";
compatible = "st,stm32mp157c-dk2", "st,stm32mp157";

chosen {
stdout-path = "serial0:115200n8";
};
};

 

Clocks measured:

Xtal connected to PHY = 25Mhz,
Clock output from PHCLK125= 125Mhz,
RX Clock frequency = 25Mhz,
TX Clock frequency = 2,5Mhz. [Why different compared to RX?]

We have some design length differences in signals from Ethernet controller to PHY, which are a in pico second range and should be within limit of the PHY:

stefboerrigter_0-1721214588691.png

 

Signal length of lines & calculated delays
NameSignal Length (mm)Delay (ps)
   
ETH1_GTX_CLK_PP1133910
ETH1_MDC_PP1144990
ETH1_MDIO_PP11531052
ETH1_RXD0-NetR1003_2_PP1137935
ETH1_RXD1-NetR1002_2_PP1143974
ETH1_RXD2-NetR1001_2_PP1121799
ETH1_RXD3-NetR1000_2_PP11621110
ETH1_RX_CLK-NetR1004_2_PP11601098
ETH1_RX_CTL-NetR1005_2_PP1126833
ETH1_TXD0_PP11881294
ETH1_TXD1_PP11551038
ETH1_TXD2_PP11811239
ETH1_TXD3_PP12051400
ETH1_TX_CTL_PP1121808
ETH_CLK125OUT-NetR1006_2_PP11551058
ETH_GPIO2-NetR1044_1_PP12031407
ETH_GPIO3-NetR1037_1_PP11691163
ETH_GPIO4-NetR1038_1_PP11601101
ETH_GPIO5-NetR1039_1_PP1131867
ETH_RESET_N-NetC1033_2_PP1144982

 

5 REPLIES 5
stefboerrigter
Associate II

Note; we have updated the table with the delays for better understandability:
Please note the column "Delay Datalines VS clock (ps)" for absolute delay in ps related to shortest path (RX lines compared to RXC and TX lines compared to TXC). 

Info

Name

Signal Length (mm)

Routed Length (mm)

Delay (ps)

Delay (ps) 

Delay Datalines Delta (ps) 

Delay Datalines VS clock (ps)

Delta length (mm)

RXD0

ETH1_RXD0-NetR1003_2_PP1

137.343

137.343

935.370

935,37

135,945

163

15.818

RXD1

ETH1_RXD1-NetR1002_2_PP1

143.291

143.291

974.614

974,614

175,189

124

21.766

RXD2

ETH1_RXD2-NetR1001_2_PP1

121.525

121.525

799.425

799,425

0

299

0

RXD3

ETH1_RXD3-NetR1000_2_PP1

162.812

162.812

1.110.454

1110,454

311,029

12

41.287

RXC

ETH1_RX_CLK-NetR1004_2_PP1

160.531

160.531

1.098.753

1098,753

 

0

39.006

RX_CTL

ETH1_RX_CTL-NetR1005_2_PP1

126.011

126.011

833.283

833,283

 

 

4.486

TX

Tx Deltas:

 

 

 

 

 

 

 

TXD0

ETH1_TXD0_PP1

188.738

188.738

1.294.866

1294,866

256,574

384

66.870

TXD1

ETH1_TXD1_PP1

155.307

155.307

1.038.292

1038,292

0

128

33.439

TXD2

ETH1_TXD2_PP1

181.008

181.008

1.239.061

1239,061

200,769

328

59.140

TXD3

ETH1_TXD3_PP1

205.391

205.391

1.400.498

1400,498

362,206

490

83.523

TXC

ETH1_GTX_CLK_PP1

133.627

133.627

910.679

910,679

 

0

11.759

TX_CTL

ETH1_TX_CTL_PP1

121.868

121.868

808.406

808,406

 

 

0

stefboerrigter
Associate II

Update after some investigation
1. We have modified our board (reverted basically) to NOT use the 125MHz from the Phy. We have enabled in TF-A & OP-Tee the 

 

CLK_ETH_PLL4P

 

which is configured for 125Mhz via the HSE (24MHz) divmn = <3, 124>; st,pll_div_pqr=<5 7 7>; 

2. In Kernel DTS we enable the st,eth-clk-sel so taht in dwmac-stm32.c during 'stm32mp1_set_mode'  in RGMII mode the enable_eth_ck is activated. We have briefly checked with 25Mhz clock but that doesn't seem to work (get DMA issues reported in dmesg again).

stefboerrigter_0-1721744543689.png

(Relevant) Dmesg output:

 

root@wesl:~# dmesg | grep eth -i [ 0.000000] psci: probing for conduit method from DT. [ 0.269579] pegasus: Pegasus/Pegasus II USB Ethernet driver [ 0.269869] usbcore: registered new interface driver cdc_ether [ 0.289639] optee: probing for conduit method. [ 1.633461] stm32-dwmac 5800a000.ethernet: IRQ eth_lpi not found [ 1.638406] stm32-dwmac 5800a000.ethernet: SB: ETH Clock is selected [ 1.644698] stm32-dwmac 5800a000.ethernet: no regulator found [ 1.645213] stm32-dwmac 5800a000.ethernet: User ID: 0x40, Synopsys ID: 0x42 [ 1.651507] stm32-dwmac 5800a000.ethernet: DWMAC4/5 [ 1.656380] stm32-dwmac 5800a000.ethernet: DMA HW capability register supported [ 1.663688] stm32-dwmac 5800a000.ethernet: RX Checksum Offload Engine supported [ 1.670992] stm32-dwmac 5800a000.ethernet: TX Checksum insertion supported [ 1.677790] stm32-dwmac 5800a000.ethernet: Wake-Up On Lan supported [ 1.684208] stm32-dwmac 5800a000.ethernet: TSO supported [ 1.689404] stm32-dwmac 5800a000.ethernet: Enable RX Mitigation via HW Watchdog Timer [ 1.697220] stm32-dwmac 5800a000.ethernet: Enabled L3L4 Flow TC (entries=2) [ 1.704109] stm32-dwmac 5800a000.ethernet: Enabled RFS Flow TC (entries=10) [ 1.711128] stm32-dwmac 5800a000.ethernet: TSO feature enabled [ 1.716923] stm32-dwmac 5800a000.ethernet: Using 32/32 bits DMA host/device width [ 4.790153] stm32-dwmac 5800a000.ethernet eth0: Register MEM_TYPE_PAGE_POOL RxQ-0 [ 4.798399] stm32-dwmac 5800a000.ethernet eth0: PHY [stmmac-0:00] driver [Generic PHY] (irq=POLL) [ 4.811330] stm32-dwmac 5800a000.ethernet eth0: No Safety Features support found [ 4.818694] stm32-dwmac 5800a000.ethernet eth0: IEEE 1588-2008 Advanced Timestamp supported [ 4.827408] stm32-dwmac 5800a000.ethernet eth0: registered PTP clock [ 4.836131] stm32-dwmac 5800a000.ethernet eth0: configuring for phy/rgmii link mode [ 4.847854] stm32-dwmac 5800a000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off [ 4.854815] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

 

 Status

  • Interface is up and responsive. It doesn't crash and detects a link automatically via Autonegotiate as expected.
  • Data transfer DOESN't work (e.g. dhcp or ping with fixed IP) never any data is passed through. 

Anyone with hints / tips what to check? 

Dump of Information:

 

root@wesl:~# ifconfig eth0 Link encap:Ethernet HWaddr 10:E7:7A:E1:85:E5 inet6 addr: fe80::12e7:7aff:fee1:85e5/64 Scope:Link UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 RX packets:0 errors:0 dropped:0 overruns:0 frame:0 TX packets:16 errors:0 dropped:0 overruns:0 carrier:0 collisions:0 txqueuelen:1000 RX bytes:0 (0.0 B) TX bytes:3120 (3.0 KiB) Interrupt:50
root@wesl:~# ethtool eth0 Settings for eth0: Supported ports: [ TP MII ] Supported link modes: 10baseT/Half 10baseT/Full 100baseT/Half 100baseT/Full 1000baseT/Full Supported pause frame use: Symmetric Receive-only Supports auto-negotiation: Yes Supported FEC modes: Not reported Advertised link modes: 10baseT/Half 10baseT/Full 100baseT/Half 100baseT/Full 1000baseT/Full Advertised pause frame use: Symmetric Receive-only Advertised auto-negotiation: Yes Advertised FEC modes: Not reported Link partner advertised link modes: 10baseT/Half 10baseT/Full 100baseT/Half 100baseT/Full 1000baseT/Full Link partner advertised pause frame use: No Link partner advertised auto-negotiation: Yes Link partner advertised FEC modes: Not reported Speed: 1000Mb/s Duplex: Full Auto-negotiation: on master-slave cfg: preferred slave master-slave status: master Port: MII PHYAD: 0 Transceiver: external Supports Wake-on: ug Wake-on: d Current message level: 0x0000003f (63) drv probe link timer ifdown ifup Link detected: yes root@wesl:~#
View more
root@wesl:~# cat /sys/kernel/debug/clk/clk_summary | grep eth ethstp 0 0 0 266500000 0 0 50000 N ethmac 1 1 0 266500000 0 0 50000 Y ethtx 1 1 0 266500000 0 0 50000 Y ck_ker_eth 2 2 0 125000000 0 0 50000 Y ethptp_k 1 1 0 125000000 0 0 50000 Y ethck_k 2 2 0 125000000 0 0 50000 Y ethrx 1 1 0 125000000 0 0 50000 Y

 

mdio tool shows 2 phys (reporting on addr 4 AND addr 0)

 

root@wesl:~# mdio stmmac-0 DEV PHY-ID LINK 0x00 0x00221652 up 0x04 0x00221652 up
oot@wesl:~# phytool eth0/0 ieee-phy: id:0x00221652 ieee-phy: reg:BMCR(0x00) val:0x1040 flags: -reset -loopback +aneg-enable -power-down -isolate -aneg-restart -collision-test speed: 1000-half ieee-phy: reg:BMSR(0x01) val:0x796d capabilities: -100-b4 +100-f +100-h +10-f +10-h -100-t2-f -100-t2-h flags: +ext-status +aneg-complete -remote-fault +aneg-capable +link -jabber +ext-register

 

Hi,

maybe a basic info:

For RGMII, did you enabled the ~2ns delay on RX and TX inside the PHY (sometimes it is thru HW config, sometimes thru MDIO SW control with device tree) ?

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
stefboerrigter
Associate II

Thanks @PatrickF .

We have not set any delay specifically. we just copied the implemenation from the DK boards. 
Also not sure if the path differences is wrong, according to the datasheet it is below <1ns differenence, therefore not a problem? but we can test if you give me some more info.

What we do notice, and are not sure about is the difference in TX and RX clock. We see in Linux that the RX and TX clock have different sources (and frequencies), and also when we measure them they are significantly different.
The RX clock is a nice 125MHz clock, but TX seems to be jittering all over the place (or we cannot measure it correctly). 

Hi,

delay on RGMII is a must, it could be either on GMAC or PHY side, but as STM32MP1 does not have embedded delay on neither RX or TX direction, it must be enabled on the PHY side for RX and TX (depend on the PHY driver I guess).

PatrickF_0-1721747670145.png

 

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.