2022-12-23 9:47 PM
we are working on STM32MP1 in UBOOT 2018 version .
we are trying to access the EMMC from UBOOT by using following commands in the below link
https://develop.phytec.com/phycore-imx7/linux/pd18.1.0/how-to-guides/flashing-and-booting-from-emmc
EMMC is device detecting, but while writing image into EMMC device is getting hanged.
so we are unable to write image into EMMC.
Please help us in this regards.
2022-12-24 6:36 AM
Is this a custom board?
Is there a mismatch between the image size and the eMMC capacity?
2022-12-25 8:16 PM
Hi ,
thanks for the reply.
yes, we are using stm32mp157a processor in my custom board. EMMC capacity is 8bit and image size is fine.
2023-01-03 8:53 AM
Hi @Navaneeth kumar
The link you provided is for NXP product, not sure it will work very same for STM32MP1.
What about using CubeProgrammer ? Any messages ?
Populating eMMC is very similar than SD-Card, just use relevant flashlayout file.
See also https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer
and https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer_flashlayout#e-E2-80-A2MMC
Regards.
In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'