2020-03-03 08:34 AM
Dear STM32 MPU Community,
We are please to announce that New MP1 Ecosystem V1.2.0 ! is available since the 25th of February 2020.
This is version of each component of this release and features to be highlighted ( most expected in this community ) :
Openstlinux-20-02-19 :
see https://wiki.st.com/stm32mpu/wiki/Package_repository_for_OpenSTLinux_distribution
STM32CubeMP1-v1.2.0 :
STM32CubeProgrammer-v2.4.0 :
STM32CubeMX-v5.6 :
STM32CubeIDE V1.3.0 :
Refer to https://wiki.st.com/stm32mpu/index.php/STM32MP15_ecosystem_release_note
for complete description and download.
Major Update on Wiki Documentation !
As usual, Ecosystem release has been opportunity to update and enrich the Wiki Online User Document !
Please visit https://wiki.st.com/stm32mpu/wiki/Main_Page
Hope you will enjoy this new release.
Looking forward to read you on this Community !
2020-03-14 11:10 AM
Hi,
Can I install python package using ecosystem-release-v12 on STM32MP1DK2? Is X-LINUX-AI-CV OpenSTLinux expansion package is compatible with this release?
I am looking for python package response, json etc. In Linux, we can install package using pip install "package name". Is this also possible with this latest release?
If not then can you please share other alternatives?
Thanking you,
Saurabh
2020-03-16 12:51 AM
Sorry I resolved the above problem. Please ignore it.
2020-07-21 08:34 AM
How did you solved the problem? Can you please elaborate ? I also need to have git and python installed.