2023-01-24 07:28 AM
Hi!
I am using STM32MP157C-DK2 board to create an application on the screen (using GTK library). My idea is to start coprocessor firmware from the A7 application with the following commands (system commands):
int main (int argc, char **argv)
{
GtkApplication *app;
system("su root -c 'echo core_communication_new_CM4.elf' > /sys/class/remoteproc/remoteproc0/firmware");
system("su root -c 'echo start' > /sys/class/remoteproc/remoteproc0/state");
app = gtk_application_new ("org.gtk.example", G_APPLICATION_FLAGS_NONE);
g_signal_connect (app, "activate", G_CALLBACK (Window_info), NULL);
status = g_application_run (G_APPLICATION (app), argc, argv);
g_object_unref (app);
return status;
}
With these two system commands, I want to boot the M4 firmware (core_communication_new_CM4.elf). Then, I initialize A7 program (probak_GTK) with the following command:
However, when I run the A7 application, I get the following message in the Linux terminal:
Does anyone know how I can boot M4 firmware from A7 application?
Thanks!
Solved! Go to Solution.
2023-02-01 11:46 PM
Hello @TArre.1 ,
My bad, the test from my side was wrong.
In fact, since DV 4.0, all the graphical part needs to be launched by a user session (which is "weston" in our case). But when you run your program as "weston", it is logical to not have access to root privilege for security reasons.
So I think all will depend about your use case:
I hope that these different lines of thought will help you to go forward.
Kind regards,
Erwan.
2023-01-24 08:23 AM
Hello @TArre.1 ,
This issue is mainly due to the fact that a weston profile cannot access to su rights. This is what happens when you call your "system()" function.
But remember, everything is file in Linux ! It means that when you do an echo start > file , you just write the word "start" in the file.
Based on this, try to play with fopen(), fprintf() and fclose() functions to write directly what you want in your different files to launch the copro, instead of using the system() function, which is quite ugly by the way 😉
Kind regards,
Erwan
2023-01-25 01:36 AM
Hi @Erwan SZYMANSKI thank you for your reply 😀
I am trying to use your functions (fopen(), fprintf() and fclose()) with the following code:
FILE* fd;
// SET FIRMWARE
g_print("Set firmware\n");
fd = fopen("/sys/class/remoteproc/remoteproc0/firmware", "w");
if (fd == NULL)
{
g_print("Error opening file\n");
return -1;
}
g_print("Firmaware has been opened\n");
fprintf(fd, "core_communication_new_CM4.elf");
fclose(fd);
However, I am unable to open the file and get the same error:
I do not know if in weston I can not configure the firmware in the coprocessor or I am doing something wrong.
2023-02-01 12:11 AM
Hello @TArre.1,
Sorry for the delay of my answer.
Do you still have your issue ?
Can you try to launch you application like this just to compare ?
> cd /usr/local
> su weston
> su -c './probak_GTK'
Kind regards,
Erwan.
2023-02-01 07:38 AM
Hi @Erwan SZYMANSKI
I have tried starting with your command with the following error:
It seems that:
So I do not know if there is an option to do both together.
Thanks!
2023-02-01 11:46 PM
Hello @TArre.1 ,
My bad, the test from my side was wrong.
In fact, since DV 4.0, all the graphical part needs to be launched by a user session (which is "weston" in our case). But when you run your program as "weston", it is logical to not have access to root privilege for security reasons.
So I think all will depend about your use case:
I hope that these different lines of thought will help you to go forward.
Kind regards,
Erwan.
2023-02-10 12:49 AM
Hi @Erwan SZYMANSKI
I'll try to start the coprocessor from the beginning as it may work for my application.
Thank you for your explanation.😁
Telmo