cancel
Showing results for 
Search instead for 
Did you mean: 

Request for Recommendations on 64-bit ARM Development Boards

Vista123
Associate II

Hi,

I am looking to design a board based on a 64-bit ARM processor, with interfaces including USB, Serial, and Ethernet. Could you kindly suggest any development boards that could serve as a good reference for this project?

Your recommendations would be greatly appreciated.

 

Thank You

1 REPLY 1
TDK
Guru

I believe this is the only 64-bit chip from ST:

STM32MP2 series - STMicroelectronics

 

Also on the way:

STM32MP25: 1st STM32 MPU with 1.35 TOPS NPU and 64-bit cores #STM32Summit

If you feel a post has answered your question, please click "Accept as Solution".