2024-05-15 10:48 AM
Hi everyone,
recently we have developed a custom board based on stm32mp157 mpu. We have used openstlinux distribution and the branch is "kirkstone". Ethernet is working perfectly on the Linux kernel. But problem arises when I am in the uboot mode (We want to have access to the ethernet from uboot). First, the ethernet can not find the mac address. It shows the following Error:
invalid MAC address 0 in OTP 00:00:00:00:00:00
Error: ethernet@5800a000 address not set.
No ethernet found.
EQOS_DMA_MODE_SWR stuck FAILED: -110 in stm32mp157 for u-boot
I have the following configuration for the ethernet in uboot device tree.
ðernet0{
pinctrl-names = "default", "sleep";
pinctrl-0 = <ð1_pins_mx>;
pinctrl-1 = <ð1_sleep_pins_mx>;
status ="okay";
/* USER CODE BEGIN ethernet0 */
phy-mode = "rmii";
max-speed = <100>;
phy-handle = <&phy0>;
phy-supply = <&vdd_usb>;
nvmem-cells = <ðernet_mac_address>;
nvmem-cell-names = "mac-address";
clock-names = "stmmaceth",
"mac-clk-tx",
"mac-clk-rx",
"ethstp",
"eth-ck",
"syscfg-clk";
clocks = <&rcc ETHMAC>,
<&rcc ETHTX>,
<&rcc ETHRX>,
<&rcc ETHSTP>,
<&rcc ETHCK_K>,
<&rcc SYSCFG>;
st,eth_ref_clk_sel;
phy-reset-gpios = <&gpiob 0 GPIO_ACTIVE_LOW>;
mdio0 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "snps,dwmac-mdio";
phy0: ethernet-phy@0 {
reset-gpios = <&gpiob 0 GPIO_ACTIVE_LOW>;
reset-duration = <200>;
reg = <0>;
};
};
/* USER CODE END ethernet0 */
};
Can anyone help me to solve those above two errors? Thanks in advance.
Solved! Go to Solution.
2024-05-24 03:31 AM
Finally got the solution for the Error. This Error basically indicate the clock issue. EQOS_DMA_MODE_SWR function is being called if software reset is not done in the SWR time interval. I set the wrong clock. I figured it out by measuring the clock using oscilloscope.
2024-05-17 04:28 AM
I got solution for the the first problem in defconfig I added "CONFIG_NET_RANDOM_ETHADDR=y".
Which is getting a random mac address. Now I do not have to set the mac address manually. But still I have the second error and can not establish the connection with the internet.
2024-05-24 03:31 AM
Finally got the solution for the Error. This Error basically indicate the clock issue. EQOS_DMA_MODE_SWR function is being called if software reset is not done in the SWR time interval. I set the wrong clock. I figured it out by measuring the clock using oscilloscope.